Power & Energy
  • Technologies
  • More
Power & Energy
Forum Raising the voltage to use a photocell
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 35 replies
  • Answers 1 answer
  • Subscribers 287 subscribers
  • Views 5075 views
  • Users 0 members are here
  • solar-powered
  • Alternative Energy Tags
Related

Raising the voltage to use a photocell

e14 Contributor
e14 Contributor over 12 years ago

Anyone know how can i raising the voltage of a photocell?, from 0.5 volts to 5 volts, the photocell give me 0.5 volts and 9 amp, the problem is that if i use operational amplifier, i don't have the power to energize a small engine, i appreciate any information that  could be usefull or component that resist the power.image

¿Alguien sabe como puedo utilizar esta celda solar?, entrega 0.5 v y 9 amp, por ende la potencia es de 4.5 Watts, necesito subir el voltaje a 5 V aunque se reduzca la corriente, pero los diseños con operacionales no me resultan funcionales ya que tendria que darme alrededor de medio amper, y no resisten la corriente, ¿tienen alguna idea de como puedo hacerlo?

  • Sign in to reply
  • Cancel
Parents
  • johnbeetem
    0 johnbeetem over 12 years ago

    I think what you want to look for is a boost-mode switching regulator also known as a step-up DC-to-DC converter.  They use an external inductor or transformer to boost a small input voltage.  For example, here's a Linear Technology LTC3105 which takes input from 0.25 to 5.0V and produces 1.5V to 5.25V.  However, this particular part doesn't produce much current with a 0.5V input, and its efficiency at that input voltage is poor, so I'm showing this as the kind of part to look for.  TI and Maxim also offer these kinds of parts.

     

    The Linear Tech page has some articles on solar energy harvesting showing what you can expect from solar cells.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • johnbeetem
    0 johnbeetem over 12 years ago

    I think what you want to look for is a boost-mode switching regulator also known as a step-up DC-to-DC converter.  They use an external inductor or transformer to boost a small input voltage.  For example, here's a Linear Technology LTC3105 which takes input from 0.25 to 5.0V and produces 1.5V to 5.25V.  However, this particular part doesn't produce much current with a 0.5V input, and its efficiency at that input voltage is poor, so I'm showing this as the kind of part to look for.  TI and Maxim also offer these kinds of parts.

     

    The Linear Tech page has some articles on solar energy harvesting showing what you can expect from solar cells.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to johnbeetem

    Thanks John i never hear about that divice, i hope i can get one here in mexico,i'm visiting de web site to check the logistic sending for a few devices.