Power & Energy
  • Technologies
  • More
Power & Energy
Forum Raising the voltage to use a photocell
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 35 replies
  • Answers 1 answer
  • Subscribers 286 subscribers
  • Views 5085 views
  • Users 0 members are here
  • solar-powered
  • Alternative Energy Tags
Related

Raising the voltage to use a photocell

e14 Contributor
e14 Contributor over 12 years ago

Anyone know how can i raising the voltage of a photocell?, from 0.5 volts to 5 volts, the photocell give me 0.5 volts and 9 amp, the problem is that if i use operational amplifier, i don't have the power to energize a small engine, i appreciate any information that  could be usefull or component that resist the power.image

¿Alguien sabe como puedo utilizar esta celda solar?, entrega 0.5 v y 9 amp, por ende la potencia es de 4.5 Watts, necesito subir el voltaje a 5 V aunque se reduzca la corriente, pero los diseños con operacionales no me resultan funcionales ya que tendria que darme alrededor de medio amper, y no resisten la corriente, ¿tienen alguna idea de como puedo hacerlo?

  • Sign in to reply
  • Cancel
Parents
  • D_Hersey
    0 D_Hersey over 12 years ago

    Why not just stack a few of the photocells?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • D_Hersey
    0 D_Hersey over 12 years ago

    Why not just stack a few of the photocells?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to D_Hersey

    I need to used only one or two cell, because we don't have a lot of space to mounting, and for not raise de production cost,if i stack a few photocell i'll need ten to have five volts.But thanks for the opinion.