Power & Energy
  • Technologies
  • More
Power & Energy
Forum Can I power 3 components (video game, LCD screen and audio amp) with a small 6 volt adaptor?
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 281 subscribers
  • Views 708 views
  • Users 0 members are here
  • video
  • power_management
  • diy
  • battery
  • gaming
  • power
Related

Can I power 3 components (video game, LCD screen and audio amp) with a small 6 volt adaptor?

e14 Contributor
e14 Contributor over 12 years ago

I'm building a small desktop video arcade system using one of those old Namco Joystick boxes which are battery driven (4 AA batteries) and have an audio and video RCA jack which you hook up directly to a tv.

 

There are 3 main components.

 

Video Game/joystick box

http://www.ebay.com/itm/Namco-Pacman-Galaxian-Dig-Dug-5-in-1-TV-Video-Game-Plug-and-Play-Jakks-2003-/181443728782?pt=Games_US&hash=item2a3ee3958e

Regarding the power requirements. All I know is that it takes 4 AA batteries. So 6 volts. I don't know how much current it draws. Can I use a multimeter to measure this? Do I need this information to move forward?

 

4 Inch LCD Video Screen

Amazon.com : 4.3 Inch LCD TFT Rearview Monitor screen for Car Backup Camera : Vehicle Backup Cameras : Car Electronics

Here is the range of power options for this device.

Voltage/Current/Power

5.1v / .27a / 1.377w [lowest stable voltage]

6.0v / .25a / 1.5w

6.6v / .23a / 1.518w

7.4v / .20a / 1.48w

8.0v / .18a / 1.44w

8.6v / .17a / 1.462w

9.2v / .16a / 1.472w

9.8v / .15a / 1.47w

10.4v / .14a / 1.456w

11.0v / .13a / 1.43w

11.6v / .12a / 1.392w

12.0v / .12a / 1.44w [highest recommended voltage]

 

Small Audio App Chip to drive a small speaker. Probably not more that 1 watt I'm guessing would be loud enough.

Not sure what to use here. Any ideas? If this also can take 6 volts then everything can be powered by one 6 volt power supply.

 

I've already built one of these (see below) but ended up using both the video game batteries (which powered the video game) and a separate 12 volt power supply (which powered both the LCD and an audio amp board) and I didn't like that as you had to replace the batteries as well as have it plugged in all the time. I ended up using a small 3 watt amplifier which was WAY too powerful. I could only turn it up a little before the volume was earth shattering. And this was a 3.5 audio amplifier board which cost about $12.  I would prefer it to be as simple and inexpensive as possible. Just need to amplify the RCA audio output to levels appropriate to playing on a kitchen table. Not very loud.

 

Ideally I would like to:

 

  • Power all three things with the (4 AA batteries) that comes with the joystick. That would be ideal as it would allow this small video arcade machine to be portable. Assuming though that the batteries didn't drain way too fast.
  • If the batteries don't provide enough current then the next best thing would be a power adaptor. Something like this assuming that it could power all three components (video game/joystick, video screen and audio amplifier).  Amazon.com: 6V 1A AC Adapter to dc Power Adapter 5.5/2.1mm: Electronics

 

Once I have the parts worked out I'm going to teach a DIY class to 5-10 young under-privileged kids where they can put their own arcade machine together. I'm hoping to keep the costs down to under $50 as I will have be self-funding this.

 

So my issues are:

  • Can I power all this with one power supply?
  • Can you recommend a small audio amplifier. Preferably less than $8 or so. I'm trying to keep the parts under $50.
  • And are there issues like voltage spiking that I have to worry about when connecting multiple components like this to one power supply? Or can I just hook them up in parallel assuming they all take 6 volts and the total current draw is less than the power adapter is rated?

 

Any help you could give me would be greatly appreciated.

 

Here's my first attempt from last year. I like it a lot except for the power supply issues.

http://www.jochumson.com/project7.html

image

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    To measure how much current a circuit draws set your multimeter to the amp setting and connect one wire from your power source to your device and use your multimeter to complete the circuit by touching one probe of your meter to the wire not connected to you circuit and the other side the power supply and your meter will display the current draw. To answer you question about powering your three devices with one power supply follow the previous steps for all three devices and add your current draws together and if the resulting number is lower than the amp rating on your 6v power supply it will be able to supply the correct amount of power for your project.image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    To measure how much current a circuit draws set your multimeter to the amp setting and connect one wire from your power source to your device and use your multimeter to complete the circuit by touching one probe of your meter to the wire not connected to you circuit and the other side the power supply and your meter will display the current draw. To answer you question about powering your three devices with one power supply follow the previous steps for all three devices and add your current draws together and if the resulting number is lower than the amp rating on your 6v power supply it will be able to supply the correct amount of power for your project.image