Power & Energy
  • Technologies
  • More
Power & Energy
Forum Not sure what batteries to use for a project.
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 285 subscribers
  • Views 727 views
  • Users 0 members are here
  • batteries
  • recharge
  • battery
  • 12
  • volt
  • power
  • rechargable
Related

Not sure what batteries to use for a project.

e14 Contributor
e14 Contributor over 12 years ago

So I am making a portable netflix laptop and I need to use a small, rechargeable 12v battery to power it. It would need to have enough power to power a small 7" lcd display and a Netflix streaming device. They both run off of 12v.(Lucky me) I have not found any batteries that are reasonably priced, and are too big. They need to be around 7" x 1.5" x 1.5" or something around that. I also need to know how I would recharge them. If you could maybe give me a link to some inexpensive 12v batteries and a way of charging them, that would be great.

 

Thanks.

  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 12 years ago in reply to vaghasiamadhuri +1
    The RC Hobby batteries contain no protection for over current discharge or over charging. Try to look for ones that are less than 2C and include protection. The same suppliers usually have chargers to…
  • e14 Contributor
    e14 Contributor over 12 years ago +1
    Try Googling the battery type mcb1 said and you may find some results.
  • D_Hersey
    D_Hersey over 12 years ago +1
    Buck convertors buck, or provide less potential than the input. Because the lithium polymer battery potential can be above or below what is desired, second-order topologies such as SEPIC are used with…
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Try Googling the battery type mcb1 said and you may find some results.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Try Googling the battery type mcb1 said and you may find some results.