Power & Energy
  • Technologies
  • More
Power & Energy
Forum garden lanterns' solar panel help needed
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 283 subscribers
  • Views 1262 views
  • Users 0 members are here
  • lantern
  • solar-panel
  • solar
Related

garden lanterns' solar panel help needed

hafcanadian
hafcanadian over 12 years ago

I'm new to learning circuitry, so forgive any ignorance that I may reveal

 

I've got several solar yard lanterns of various sizes that I've accumulated over the last 10-15 years.  Some are classical, some have an amber glow, some "flicker" like a candle, and some are modern with bright white LED's that have little staying power and dim within a few hours after nightfall.  Out of about 10 of them, only 4 still function, and two of those have to have their AA batteries recharged manually in order to work.  Some of the others might work if charged batteries were inserted, but I haven't tried them all;  running around the yard each evening removing dead batteries and installing fresh Nicads or Nihydrides just isn't plausible.

 

Lately the oldest lantern, heretofore very reliable, has started failing as well, so every several days I replace its rechargeables with fresh ones charged in the house.  In all cases I can see the solar collection panel on the top (some newer lanterns have 4 panels) has deteriorated.  The surface of the panels loose their smoothness and polished shine, but below the surface the visible pathways have dimmed and discolored.  The oldest (and most favorite) has worked flawlessly for 10 years or more until now, whereas others I've bought lasted only a few months before summer sun faded their panels to an inoperative state.  The manufacturer sent replacements that have lasted several years, but one of those is acting up this season, and they never asked for the 2 original lanterns back so I still have them.

 

I'd like to replace the faded and faulty panels and get as many yard lanterns up and running again as possible.  It's obvious that in almost all instances the problem comes from failed or failing solar panels, although some circuit boards aren't in the best condition;  they are outside afterall, exposed to moisture and spider activity.  The lanterns were made by various companies, some of which no longer exist, and all of whom will not replace panels.  They are bulk-made in China - the market has no room for parts provision as a customer service.

 

Can anyone advise me on a source for replacing the various types and formats of small garden lantern solar panels?  I'm sure there will have to be some consideration for electrical output capacity as well as physical size, but I should be able to get that information for each lantern off its battery pack, circuit board, or instruction sheet if I still have it.  I'm still unclear as to whether I'll need to be careful which battery type to use - the oldest ones use Ni-Cads, the newest ones use NiMh;  I know I have to use the proper charger for each in the house, but can the older lanterns charge NiMH?  Ni-Cads are getting hard to find in stores anyway.  I need resources for obtaining decent panels though.  From the two units that faded and failed within a couple of months in the sun, I can tell there's junk or poorly coated panels out there I need to avoid.

 

Thanks for any help.

-hafcanadian

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 12 years ago +1
    Hi Joel I have taken several different kinds of lawn lamps apart and looked at the circuits. In all cases it is a 2 volt solar panel that feeds through a voltage sensitive solid state switch. When the…
Parents
  • shabaz
    0 shabaz over 12 years ago

    Generally it is hard to suggest replacements that are not identical, because it is guesswork what the original designer intended. For example NiCd cells have a different end-of-charge detection than NiMH (NiMH has a different voltage gradient preceding charge termination, from memory, and for NiCd various designers may use different methods, such as change in voltage, or temperature gradient, or combination). Without a circuit diagram (which only the manufacturer is likely to have) it is not easy to know. A simple garden device might just trickle charge however - it's the most likely scenario. It's safer and more likely to work for another 10 years if replaced with similar cells, i.e. NiCd and not NiMH.

    Farnell do sell solar panels, however they may be too large. This leaves you with scouring hobby electronics sites or ebay unfortunately, for something approximately the same size so it can fit. In theory solar cells should last for 20 years or more if assembled well. 10 years is quite good for a garden lamp. There are a few different types of solar cells, some more efficient, but it may come down to cost.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 12 years ago

    Generally it is hard to suggest replacements that are not identical, because it is guesswork what the original designer intended. For example NiCd cells have a different end-of-charge detection than NiMH (NiMH has a different voltage gradient preceding charge termination, from memory, and for NiCd various designers may use different methods, such as change in voltage, or temperature gradient, or combination). Without a circuit diagram (which only the manufacturer is likely to have) it is not easy to know. A simple garden device might just trickle charge however - it's the most likely scenario. It's safer and more likely to work for another 10 years if replaced with similar cells, i.e. NiCd and not NiMH.

    Farnell do sell solar panels, however they may be too large. This leaves you with scouring hobby electronics sites or ebay unfortunately, for something approximately the same size so it can fit. In theory solar cells should last for 20 years or more if assembled well. 10 years is quite good for a garden lamp. There are a few different types of solar cells, some more efficient, but it may come down to cost.