Power & Energy
  • Technologies
  • More
Power & Energy
Forum garden lanterns' solar panel help needed
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 283 subscribers
  • Views 1260 views
  • Users 0 members are here
  • lantern
  • solar-panel
  • solar
Related

garden lanterns' solar panel help needed

hafcanadian
hafcanadian over 12 years ago

I'm new to learning circuitry, so forgive any ignorance that I may reveal

 

I've got several solar yard lanterns of various sizes that I've accumulated over the last 10-15 years.  Some are classical, some have an amber glow, some "flicker" like a candle, and some are modern with bright white LED's that have little staying power and dim within a few hours after nightfall.  Out of about 10 of them, only 4 still function, and two of those have to have their AA batteries recharged manually in order to work.  Some of the others might work if charged batteries were inserted, but I haven't tried them all;  running around the yard each evening removing dead batteries and installing fresh Nicads or Nihydrides just isn't plausible.

 

Lately the oldest lantern, heretofore very reliable, has started failing as well, so every several days I replace its rechargeables with fresh ones charged in the house.  In all cases I can see the solar collection panel on the top (some newer lanterns have 4 panels) has deteriorated.  The surface of the panels loose their smoothness and polished shine, but below the surface the visible pathways have dimmed and discolored.  The oldest (and most favorite) has worked flawlessly for 10 years or more until now, whereas others I've bought lasted only a few months before summer sun faded their panels to an inoperative state.  The manufacturer sent replacements that have lasted several years, but one of those is acting up this season, and they never asked for the 2 original lanterns back so I still have them.

 

I'd like to replace the faded and faulty panels and get as many yard lanterns up and running again as possible.  It's obvious that in almost all instances the problem comes from failed or failing solar panels, although some circuit boards aren't in the best condition;  they are outside afterall, exposed to moisture and spider activity.  The lanterns were made by various companies, some of which no longer exist, and all of whom will not replace panels.  They are bulk-made in China - the market has no room for parts provision as a customer service.

 

Can anyone advise me on a source for replacing the various types and formats of small garden lantern solar panels?  I'm sure there will have to be some consideration for electrical output capacity as well as physical size, but I should be able to get that information for each lantern off its battery pack, circuit board, or instruction sheet if I still have it.  I'm still unclear as to whether I'll need to be careful which battery type to use - the oldest ones use Ni-Cads, the newest ones use NiMh;  I know I have to use the proper charger for each in the house, but can the older lanterns charge NiMH?  Ni-Cads are getting hard to find in stores anyway.  I need resources for obtaining decent panels though.  From the two units that faded and failed within a couple of months in the sun, I can tell there's junk or poorly coated panels out there I need to avoid.

 

Thanks for any help.

-hafcanadian

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 12 years ago +1
    Hi Joel I have taken several different kinds of lawn lamps apart and looked at the circuits. In all cases it is a 2 volt solar panel that feeds through a voltage sensitive solid state switch. When the…
Parents
  • jw0752
    0 jw0752 over 12 years ago


    Hi Joel,  If you are going to try to order replacement cells from someplace other than a manufacturer you have to be aware that the solar cells used on these lights are not single cells but rather 4 cells built into one package. A single cell has only 1/2 volt and would not be able to recharge a battery. Therefore they get special packages with 4 integrated, in series, solar cells that put out 2.0 volts. This give them enough voltage to get through the internal switching circuit and still have enough voltage to charge the battery.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • hafcanadian
    0 hafcanadian over 12 years ago in reply to jw0752

    Wouldn't ya know I'd find them readily at Amazon.  Since all my lanterns use AA rechargeables, either NiCd or NiMH, I'd assume one of these 3v units would do, at least for the smaller pagodas;  the original panels look a lot like these

    Amazon.com: Small Solar Panel 3.0V 70mA with wires: Industrial & Scientific

     

    Others at Amazon are options perhaps for the other lanterns.  I just am not sure how resilient and long lasting they are, except for whatever reviewers' information on each item there may be.

     

    JOel

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • hafcanadian
    0 hafcanadian over 12 years ago in reply to jw0752

    Wouldn't ya know I'd find them readily at Amazon.  Since all my lanterns use AA rechargeables, either NiCd or NiMH, I'd assume one of these 3v units would do, at least for the smaller pagodas;  the original panels look a lot like these

    Amazon.com: Small Solar Panel 3.0V 70mA with wires: Industrial & Scientific

     

    Others at Amazon are options perhaps for the other lanterns.  I just am not sure how resilient and long lasting they are, except for whatever reviewers' information on each item there may be.

     

    JOel