Power & Energy
  • Technologies
  • More
Power & Energy
Forum Need help with battery charging
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 10 replies
  • Answers 2 answers
  • Subscribers 284 subscribers
  • Views 1203 views
  • Users 0 members are here
  • bev
  • regen
  • battery
  • hev
  • charger
Related

Need help with battery charging

e14 Contributor
e14 Contributor over 11 years ago

Hi everyone, I am working on a custom hybrid vehicle and I have designed the motor controller myself. I have a high power MOSFET doing PWM on a large brushed electric scooter motor(24v) with a relay to switch from drive to regenerative modes. This works great as it outputs a power that can charge a capacitor or get dumped into a large resistor. The thing I want to do involves charging a battery ( Its going to be NI-MH or Lith ion or some battery with decent energy weight density) the obvious problem I see with this is designing a high power battery charging circuit something that can take as much as 1kW+ at any given moment. I know its possible to do this because HEVs and EVs do this all the time with their regenerative braking function. It is of the utmost priority to be able to capture as much power during braking as possible, thus I might even add a high value capacitor to act as a buffer. Could anyone point me in the right direction for building a DC to DC battery charger that could safely dump kilowatts of power into a battery. Also I would like some recommendations for what battery type to use ( I would prefer to use a lithium something (for their high energy capacity and small size).

  • Sign in to reply
  • Cancel

Top Replies

  • D_Hersey
    D_Hersey over 11 years ago +1
    Been waiting all of my life to meet a guy whose force of will trumped the laws of physics, met a few claimants, still waiting. Expects to out-design firms that have been in business for decades for starters…
Parents
  • D_Hersey
    0 D_Hersey over 11 years ago

    NiCads are great from an electrical standpoint.  The fastest chargers monitor temperature as well as the electrical params.  NiCads need to be disposed of properly, Cd is a toxic heavy metal.  One thing one has to watch out for is they have nearly no Rth, so if nothing limits the current, nothing limits the current.  Also, they are kinda heavy, but not so much as Pb-H2SO4

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • D_Hersey
    0 D_Hersey over 11 years ago

    NiCads are great from an electrical standpoint.  The fastest chargers monitor temperature as well as the electrical params.  NiCads need to be disposed of properly, Cd is a toxic heavy metal.  One thing one has to watch out for is they have nearly no Rth, so if nothing limits the current, nothing limits the current.  Also, they are kinda heavy, but not so much as Pb-H2SO4