Power & Energy
  • Technologies
  • More
Power & Energy
Forum Need help with battery charging
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 10 replies
  • Answers 2 answers
  • Subscribers 284 subscribers
  • Views 1228 views
  • Users 0 members are here
  • bev
  • regen
  • battery
  • hev
  • charger
Related

Need help with battery charging

e14 Contributor
e14 Contributor over 12 years ago

Hi everyone, I am working on a custom hybrid vehicle and I have designed the motor controller myself. I have a high power MOSFET doing PWM on a large brushed electric scooter motor(24v) with a relay to switch from drive to regenerative modes. This works great as it outputs a power that can charge a capacitor or get dumped into a large resistor. The thing I want to do involves charging a battery ( Its going to be NI-MH or Lith ion or some battery with decent energy weight density) the obvious problem I see with this is designing a high power battery charging circuit something that can take as much as 1kW+ at any given moment. I know its possible to do this because HEVs and EVs do this all the time with their regenerative braking function. It is of the utmost priority to be able to capture as much power during braking as possible, thus I might even add a high value capacitor to act as a buffer. Could anyone point me in the right direction for building a DC to DC battery charger that could safely dump kilowatts of power into a battery. Also I would like some recommendations for what battery type to use ( I would prefer to use a lithium something (for their high energy capacity and small size).

  • Sign in to reply
  • Cancel

Top Replies

  • D_Hersey
    D_Hersey over 11 years ago +1
    Been waiting all of my life to meet a guy whose force of will trumped the laws of physics, met a few claimants, still waiting. Expects to out-design firms that have been in business for decades for starters…
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    The problem isn't what batteries to use but how to make a dc battery charger that can handle high amperage. I have not found a dc battery charger that can do this, so if anyone can help me find one or design one. I would prefer to use a lithium battery as I have a limited space to work with and want to get the best capacity available. I know there are a bunch of lithium batteries used in RC hobby applications that can charge at 5 or 6 times their rated capacity. Does anyone know how to make a battery charger that can charger directly from dc and monitor the battery. I would not hesitate to use a micro controller as I am already using one to control the motor and gas engine servos.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    The problem isn't what batteries to use but how to make a dc battery charger that can handle high amperage. I have not found a dc battery charger that can do this, so if anyone can help me find one or design one. I would prefer to use a lithium battery as I have a limited space to work with and want to get the best capacity available. I know there are a bunch of lithium batteries used in RC hobby applications that can charge at 5 or 6 times their rated capacity. Does anyone know how to make a battery charger that can charger directly from dc and monitor the battery. I would not hesitate to use a micro controller as I am already using one to control the motor and gas engine servos.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • D_Hersey
    0 D_Hersey over 11 years ago in reply to e14 Contributor

    The reason why chargers aren't as fast as you'd like are thermal.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to D_Hersey

    I guess you would like to explain how the Tesla Model S can charge to half its range in 30 minutes!

    I am aware of thermal problems but would like to be able to capture some energy during braking, This is entirely possible the Prius,Tesla, and just about every modern hybrid and electric vehicle does it.

    If you are just going to disagree with me and say it can't be done I would appreciate you just keep this to yourself because I am trying to build it.

    Besides if a Nicad battery has such a low ESR why would there be thermal problems? ESR is the main limiting factor for how fast a battery can be charged and discharged.