Power & Energy
  • Technologies
  • More
Power & Energy
Forum Need help with battery charging
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 10 replies
  • Answers 2 answers
  • Subscribers 284 subscribers
  • Views 1227 views
  • Users 0 members are here
  • bev
  • regen
  • battery
  • hev
  • charger
Related

Need help with battery charging

e14 Contributor
e14 Contributor over 12 years ago

Hi everyone, I am working on a custom hybrid vehicle and I have designed the motor controller myself. I have a high power MOSFET doing PWM on a large brushed electric scooter motor(24v) with a relay to switch from drive to regenerative modes. This works great as it outputs a power that can charge a capacitor or get dumped into a large resistor. The thing I want to do involves charging a battery ( Its going to be NI-MH or Lith ion or some battery with decent energy weight density) the obvious problem I see with this is designing a high power battery charging circuit something that can take as much as 1kW+ at any given moment. I know its possible to do this because HEVs and EVs do this all the time with their regenerative braking function. It is of the utmost priority to be able to capture as much power during braking as possible, thus I might even add a high value capacitor to act as a buffer. Could anyone point me in the right direction for building a DC to DC battery charger that could safely dump kilowatts of power into a battery. Also I would like some recommendations for what battery type to use ( I would prefer to use a lithium something (for their high energy capacity and small size).

  • Sign in to reply
  • Cancel

Top Replies

  • D_Hersey
    D_Hersey over 11 years ago +1
    Been waiting all of my life to meet a guy whose force of will trumped the laws of physics, met a few claimants, still waiting. Expects to out-design firms that have been in business for decades for starters…
Parents
  • jw0752
    0 jw0752 over 11 years ago

    Hi Jack, Part of the problem with capturing short bursts of power with batteries is that they are electrochemical in nature and as such it takes time for chemical reactions to occur over a given reaction area. Doug has correctly advised that one way to inprove the energy capture is to increase the area of the reaction with more batteries in parrallel. Don has also called your attention to the thermal problem. Heat is generated in these chemical reactions whether they are discharging a battery or recharging it. A more efficient means of rapid storage is the capacitor. There are current technology capacitors that are capable of holding multiple watts of power. There are even types with fairly low effective serial resistance that can charge fairly quickly. A bank of capacitors in parrallel with your battery might help with the stress on the battery due to peak demands of starting the vehicle moving as well as pulses from any braking energy recovery. Don't  expect a very high energy recovery from current technology. There are about 350 kW of kinetic energy in a 1 ton vehicle moving at 60 mph. If that vehicle is brought to a stop in 15 seconds I would be surprised if you could recover more than a couple kilo watts with a battery. I believe that your efficiency would improve if the braking could be spread over a longer period. Thanks to Elon Musk's patent generousity at least you can feel free to hack a Tesla and use its technology.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 11 years ago

    Hi Jack, Part of the problem with capturing short bursts of power with batteries is that they are electrochemical in nature and as such it takes time for chemical reactions to occur over a given reaction area. Doug has correctly advised that one way to inprove the energy capture is to increase the area of the reaction with more batteries in parrallel. Don has also called your attention to the thermal problem. Heat is generated in these chemical reactions whether they are discharging a battery or recharging it. A more efficient means of rapid storage is the capacitor. There are current technology capacitors that are capable of holding multiple watts of power. There are even types with fairly low effective serial resistance that can charge fairly quickly. A bank of capacitors in parrallel with your battery might help with the stress on the battery due to peak demands of starting the vehicle moving as well as pulses from any braking energy recovery. Don't  expect a very high energy recovery from current technology. There are about 350 kW of kinetic energy in a 1 ton vehicle moving at 60 mph. If that vehicle is brought to a stop in 15 seconds I would be surprised if you could recover more than a couple kilo watts with a battery. I believe that your efficiency would improve if the braking could be spread over a longer period. Thanks to Elon Musk's patent generousity at least you can feel free to hack a Tesla and use its technology.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer