Power & Energy
  • Technologies
  • More
Power & Energy
Forum Need help with battery charging
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 10 replies
  • Answers 2 answers
  • Subscribers 284 subscribers
  • Views 1221 views
  • Users 0 members are here
  • bev
  • regen
  • battery
  • hev
  • charger
Related

Need help with battery charging

e14 Contributor
e14 Contributor over 11 years ago

Hi everyone, I am working on a custom hybrid vehicle and I have designed the motor controller myself. I have a high power MOSFET doing PWM on a large brushed electric scooter motor(24v) with a relay to switch from drive to regenerative modes. This works great as it outputs a power that can charge a capacitor or get dumped into a large resistor. The thing I want to do involves charging a battery ( Its going to be NI-MH or Lith ion or some battery with decent energy weight density) the obvious problem I see with this is designing a high power battery charging circuit something that can take as much as 1kW+ at any given moment. I know its possible to do this because HEVs and EVs do this all the time with their regenerative braking function. It is of the utmost priority to be able to capture as much power during braking as possible, thus I might even add a high value capacitor to act as a buffer. Could anyone point me in the right direction for building a DC to DC battery charger that could safely dump kilowatts of power into a battery. Also I would like some recommendations for what battery type to use ( I would prefer to use a lithium something (for their high energy capacity and small size).

  • Sign in to reply
  • Cancel

Top Replies

  • D_Hersey
    D_Hersey over 11 years ago +1
    Been waiting all of my life to meet a guy whose force of will trumped the laws of physics, met a few claimants, still waiting. Expects to out-design firms that have been in business for decades for starters…
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Yes Originally I had my setup optimized to use ultra caps, As they have an incredibly low ESR and without any electrochemical reactions they can charge and discharge as fast as you can effectively put power in or out of them! The only problem I have had with ultra caps it the cost!!!!! To build a 24V array of ultra caps or any high energy cap, the cost is around $2000usd. That is simply too much for my budget. If you look at my original post I had planned on using ultra caps for their simplicity. Don I would like to apologize especially as a Mechanical and Electrical engineer with a large background in physics, I think you had misunderstood me as being too simple and stubborn. I would like to third the usage of caps! My problem still exists in transferring the energy from the caps to a battery, this still needs to be done rather quickly as the caps(even if they have a high value) can only store a fraction of the energy a battery can hold. So I will still ask for someone who is experienced with battery charge controllers to provide me with a better understanding of how a battery charger works. I would love to buy a commercial product to charge my battery but I simply can't find one that can take 24vDC and charge a 24vDC battery. I would really love to do this project with ultra caps but with their high price I am still looking for a better solution to store that much energy. I will try to get away with a couple cheap Large value caps but I know that the amount of energy that can be stored in these would be minuscule compared to the amount regenerated. I will still do some more calculations to find out. Based on the formulas for kinetic energy and potential energy in a cap.

    Believe me I am all ears for reasonable suggestions and have been engineering almost impossible feats since age 6, So I know the engineering process very well and yes arguing is key to the process! So again If anyone can help guide me to building a battery charger that can charge Lith poly batteries at something other than a snails pace(think near max pace) I would like to hear it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 11 years ago in reply to e14 Contributor

    Hi Jack - I am not an expert on Li batteries but as I understand it the control circuitry is with the battery not the charger. These batteries are sensitive to both over charging and also to being discharged too deeply. As a result the circuit cuts off discharge of the battery before it goes too low and it also allows a high current to flow when the battery begins to charge but then regulates the current down as optimal voltage is reached and finally stops the recharge completely. Not talking about Li batteries but rechargeable batteries in general you can increase charge rate by increasing the voltage that is applied by the charger. If you are talking about recharging a 24 volt battery then this means that putting a reverse polarity 30 volts on it will charge at one rate and 36 volts placed across the same battery will charge more rapidly, as the current flowing back through the internal resistance of the battery will also increase. As the charging voltage increases there are design limits in the battery that will be reached. As you mentioned batteries with low ESR will accept more current without overheating but there are limits. Most of the modern batteries have specific requirements and limits. Since everyone is impatient, the engineers design chargers to match specific battery designs to minimize charge times and still stay within safe limits. You are not likely to get specific advice on charging large rapid charge batteries or modifying chargers to push batteries beyond their design specs from people on a forum like this as no one wants to give advice that deals with conditions that might be dangerous or lethal. Once you settle on the precise battery that you intend to use you may be able to get information from the mfg. data sheet for that battery so that you can minimize the charge time safely. It is also possible that someone on the forum would be able to give specific information if they know the exact battery you will be using.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 11 years ago in reply to e14 Contributor

    Hi Jack - I am not an expert on Li batteries but as I understand it the control circuitry is with the battery not the charger. These batteries are sensitive to both over charging and also to being discharged too deeply. As a result the circuit cuts off discharge of the battery before it goes too low and it also allows a high current to flow when the battery begins to charge but then regulates the current down as optimal voltage is reached and finally stops the recharge completely. Not talking about Li batteries but rechargeable batteries in general you can increase charge rate by increasing the voltage that is applied by the charger. If you are talking about recharging a 24 volt battery then this means that putting a reverse polarity 30 volts on it will charge at one rate and 36 volts placed across the same battery will charge more rapidly, as the current flowing back through the internal resistance of the battery will also increase. As the charging voltage increases there are design limits in the battery that will be reached. As you mentioned batteries with low ESR will accept more current without overheating but there are limits. Most of the modern batteries have specific requirements and limits. Since everyone is impatient, the engineers design chargers to match specific battery designs to minimize charge times and still stay within safe limits. You are not likely to get specific advice on charging large rapid charge batteries or modifying chargers to push batteries beyond their design specs from people on a forum like this as no one wants to give advice that deals with conditions that might be dangerous or lethal. Once you settle on the precise battery that you intend to use you may be able to get information from the mfg. data sheet for that battery so that you can minimize the charge time safely. It is also possible that someone on the forum would be able to give specific information if they know the exact battery you will be using.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer