Power & Energy
  • Technologies
  • More
Power & Energy
Forum Power Raspberry Pi and Access Point
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 4 replies
  • Answers 3 answers
  • Subscribers 283 subscribers
  • Views 1050 views
  • Users 0 members are here
Related

Power Raspberry Pi and Access Point

e14 Contributor
e14 Contributor over 12 years ago

I am working on a project where I want to integrate a Raspberry Pi and a wireless access point into the same enclosure.  The AP came with a power supply with a output rating of 12V ... 2.0A.  What I am looking for is assistance designing a small board that will take power from a wall plug AC adapter and split it out so that I can power the wifi board and the Raspberry Pi from a single plug.  Here is a very rough sketch. 

 

image

I need the custom built board to be small and provide as clean of power as possible.  I'm going for reliability.  Anyone have an idea how to get this done?  I would even consider commissioning this work out to someone who is looking for a project.

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 12 years ago +1
    Hi Michael, There are off-the-shelf modules that will take the wall plug adapter voltage (make it a 12V DC wall adapter) and convert to 5V for driving the RPI. The AP can be powered directly since it is…
  • shabaz
    shabaz over 12 years ago in reply to e14 Contributor +1 suggested
    Hi Mike, The voltage is important, the devices will consume the appropriate current (amps). You need to ensure that you deliver 12V (and 5V through the DC-DC converter) with a sufficient capability so…
  • linuxengineer
    linuxengineer over 7 years ago +1 suggested
    I opensourced on Github a (largely) self-configuring AP that works with a Pi 3B+ and Pi 4. Here's the link for the Element14 Project Page: Raspberry Pi Access Point Really just need a pi, Internet connected…
Parents
  • linuxengineer
    0 linuxengineer over 7 years ago

    I opensourced on Github a (largely) self-configuring AP that works with a Pi 3B+ and Pi 4.  Here's the link for the Element14 Project Page:

     

    Raspberry Pi Access Point

     

    Really just need a pi, Internet connected router with a free port enabled for DHCP and an Ethernet cable to uplink the Pi to the router. And of course my Github repo "pi-ap" and off you go.  Only thing you might need to change is the DHCP subnet if the default (192.168.0.0/28) clashes with an existing subnet on your LAN.  HTH- Terrence Houlahan

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • linuxengineer
    0 linuxengineer over 7 years ago

    I opensourced on Github a (largely) self-configuring AP that works with a Pi 3B+ and Pi 4.  Here's the link for the Element14 Project Page:

     

    Raspberry Pi Access Point

     

    Really just need a pi, Internet connected router with a free port enabled for DHCP and an Ethernet cable to uplink the Pi to the router. And of course my Github repo "pi-ap" and off you go.  Only thing you might need to change is the DHCP subnet if the default (192.168.0.0/28) clashes with an existing subnet on your LAN.  HTH- Terrence Houlahan

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer