Power & Energy
  • Technologies
  • More
Power & Energy
Forum I am looking for a simple excel spreadsheet to calc. transformers, no. of turns, power etc.
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Answers 2 answers
  • Subscribers 284 subscribers
  • Views 2345 views
  • Users 0 members are here
  • spreadsheet
  • excel
  • transformer
  • power
Related

I am looking for a simple excel spreadsheet to calc. transformers, no. of turns, power etc.

e14 Contributor
e14 Contributor over 11 years ago

I am looking for a starter spreadsheet excel '2003' prefered to calculate transformers (home made) small amps and volts.  These are for my experiments and I want to be as accurate as possible.  I also am looking for the same for  555/556 ic's for timing.  Any help is appreciated, thanks in advance.

  • Sign in to reply
  • Cancel
Parents
  • D_Hersey
    0 D_Hersey over 11 years ago

    The analysis of t-formers has gotten a little easier since some one figured out to reflect the secondary parasitics over to the primary (or vice-versa) so they could be lumped and the t-former sorta modeled as an inductor.  As far as n turns primary, that is a trade-off between leakage inductance and parasitic capacitance, as well as mechanical and economic factors. 

     

    There are all sorts of core materials that are used in transformers because there are all kinds of frequency and bandwidth regimes in which they are employed.  Broadband transformers are different.  Signal transformers are different than power transformers.  There are T-line transformers.  Coupling transformers for impedance matching. . .

     

    Different kinds of magnet wire are available, square wire, litzendrath wire. . .

     

    There are all kind of cores and winding schemes. . .

     

    I am proud to state as a citizen of the four-star city, that the first commercial operation to make transformers in large quantities was Thoradson in Chicago.  Between the turn-of-the-century and the advent of WWII we were a high-tech capital.

     

    Transformers are darn interesting, both on paper and in the meatspace.  As a prior poster indicated you aren't gonna become a T-former wonk in a day.

     

    ============

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • D_Hersey
    0 D_Hersey over 11 years ago

    The analysis of t-formers has gotten a little easier since some one figured out to reflect the secondary parasitics over to the primary (or vice-versa) so they could be lumped and the t-former sorta modeled as an inductor.  As far as n turns primary, that is a trade-off between leakage inductance and parasitic capacitance, as well as mechanical and economic factors. 

     

    There are all sorts of core materials that are used in transformers because there are all kinds of frequency and bandwidth regimes in which they are employed.  Broadband transformers are different.  Signal transformers are different than power transformers.  There are T-line transformers.  Coupling transformers for impedance matching. . .

     

    Different kinds of magnet wire are available, square wire, litzendrath wire. . .

     

    There are all kind of cores and winding schemes. . .

     

    I am proud to state as a citizen of the four-star city, that the first commercial operation to make transformers in large quantities was Thoradson in Chicago.  Between the turn-of-the-century and the advent of WWII we were a high-tech capital.

     

    Transformers are darn interesting, both on paper and in the meatspace.  As a prior poster indicated you aren't gonna become a T-former wonk in a day.

     

    ============

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer