Power & Energy
  • Technologies
  • More
Power & Energy
Forum What is your take on converted desktop power supplys?
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Answers 2 answers
  • Subscribers 283 subscribers
  • Views 748 views
  • Users 0 members are here
Related

What is your take on converted desktop power supplys?

glh290
glh290 over 11 years ago

Title kinda says it all but let me further elaborate.

 

What is everyone's opinion on pc PSU's being converted to a bench PSU. I probably have 10's of dozens of PSU's that either been scrapped for their innards or torn from old dumpster PC's with the ones still in tact and working I'm considering making a bench power supply.

 

I have two questions one is my personal kinda need a little advice question and the other more towards what everyone thinks.

 

There is the good ol' question "what one should I use" I have supply's ranging from 100w-900w and going from zero energy efficiency to 80+ gold. So I'm wondering is should I compromise power efficiency for a little extra safety and lower wattage so I don't have an over kill bench supply, or should I go for over kill because all of my efficient supply's are 600w + .

 

The next question is what do y'all think about taking a pc supply and recycling it to a bench supply. is it worth saving the environment by recycling or would people be better off striping them down / sending them to recycling places,and then buy a brand new supply.

 

Either way I will be making a bench supply from a old PSU due to money constraints, that does not change me wanting to know your opinions, so shoot away!

 

let the comments begin!

  • Sign in to reply
  • Cancel
Parents
  • michaelkellett
    0 michaelkellett over 11 years ago

    If you need a multi-hundred watt 12V or 3.3V supply with almost no load protection then a PC supply is OK.

    Most bench supplies have adjustable output voltage and current limits. If you can live with a 0-10V supply using the PC  supply as a 12V source may work fine and save you a little money.

    For bench work you need to be able to set the current limit from 10mA to maximum within a few % - so you can protect the thing you are testing.  The output voltage needs to be adjustable but if funds are tight you can use a standard DMM to set it up and avoif paying for  a built in meter.

    I wouldn't advise trying to modify the PC supply itself because all the mains safety stuffs goes out of the window as soon as you open the case.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • michaelkellett
    0 michaelkellett over 11 years ago

    If you need a multi-hundred watt 12V or 3.3V supply with almost no load protection then a PC supply is OK.

    Most bench supplies have adjustable output voltage and current limits. If you can live with a 0-10V supply using the PC  supply as a 12V source may work fine and save you a little money.

    For bench work you need to be able to set the current limit from 10mA to maximum within a few % - so you can protect the thing you are testing.  The output voltage needs to be adjustable but if funds are tight you can use a standard DMM to set it up and avoif paying for  a built in meter.

    I wouldn't advise trying to modify the PC supply itself because all the mains safety stuffs goes out of the window as soon as you open the case.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer