Power & Energy
  • Technologies
  • More
Power & Energy
Forum Power for Desktop PC??
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 284 subscribers
  • Views 861 views
  • Users 0 members are here
Related

Power for Desktop PC??

e14 Contributor
e14 Contributor over 11 years ago

Right now our area is suffering from heavy blackouts and this got me thinking about my desktop computer now rotting away... It is just way to sad and expensive to let it go to waste. So can I power my PC computer via a 12volt car battery without the use of an power inverter?

 

Judging on most of the PC wiring it uses 5volt and 12volt also {negative} -12volt and {negative} -5volt  also there is a 3.3Volt. I included a picture I found on the net to help explain the pins there locations and designation. I hope this helps. I am looking at the ATX 24 Pin connector.  

 

Now I am a complete layman with electronics and have no idea to go about this. That said I know that most cars use onboard computers and even hard drives surely there is enough power to get a gaming computer up and going again?

 

Right now I am using a 700 Watt PSU and it is working really well. But it is no use to me when dead... and running the generator to drive my PC at midnight might be upsetting to others that want some sleep and really a power inverter feels wrong to me as the computer is build to actually use DC not AC and as we know a inverter does consume a lot to function "depending on make and model".

 

So any inexpensive MOD with easy to find parts would be a massive  help.   image

  • Sign in to reply
  • Cancel
Parents
  • D_Hersey
    0 D_Hersey over 11 years ago

    So, to illustrate, it we had a 10V supply, and a string of ten equal-valued resistors across it, the difference across each resistor would be one volt, 10/10.  We could measure many different voltages.  Reading across a pair of connected resistors would generate two volts, signum dependant upon which way the leads were applied.  If we were to sum the net of all possible readings, the result would be zero.  If we bump the supply to 20V, then each R would feature a 2V drop.

     

    This allows your beloved 555 to be a relatively stable timer WRT delta supply voltage.  The reference string (three equal resistors, giving us a tap at 1/3 and 2/3 [0/3 and 3/3 at the ends]) is ratiometric.  A higher supply potential both raises the rate at which C is charged and the threshold it must reach in order to switch the output of the 555, keeping the timing relatively constant.  Meditate on the diagram.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • D_Hersey
    0 D_Hersey over 11 years ago

    So, to illustrate, it we had a 10V supply, and a string of ten equal-valued resistors across it, the difference across each resistor would be one volt, 10/10.  We could measure many different voltages.  Reading across a pair of connected resistors would generate two volts, signum dependant upon which way the leads were applied.  If we were to sum the net of all possible readings, the result would be zero.  If we bump the supply to 20V, then each R would feature a 2V drop.

     

    This allows your beloved 555 to be a relatively stable timer WRT delta supply voltage.  The reference string (three equal resistors, giving us a tap at 1/3 and 2/3 [0/3 and 3/3 at the ends]) is ratiometric.  A higher supply potential both raises the rate at which C is charged and the threshold it must reach in order to switch the output of the 555, keeping the timing relatively constant.  Meditate on the diagram.