Power & Energy
  • Technologies
  • More
Power & Energy
Forum What is the best way to learn how to design and make SMPS transformers?
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 17 replies
  • Answers 2 answers
  • Subscribers 284 subscribers
  • Views 4606 views
  • Users 0 members are here
  • smps
  • transformer
Related

What is the best way to learn how to design and make SMPS transformers?

peterjcs23
peterjcs23 over 11 years ago

I'd like to learn about designing and making transformers for switch mode power supplies. For example if we start with an AC to isolated DC supply say 240Vac to 5V dc 1A. Is there an evaluation kit to buy? Is there a good tutorial anywhere that you have found useful? I don't want to buy a transformer I want to choose the right core and winding and understand the principles. And there are different configuration for the control circuit, I'd like to understand that too. But to begin with a simple intro scheme will do. Thanks, Peter.

  • Sign in to reply
  • Cancel

Top Replies

  • clem57
    clem57 over 11 years ago +1 suggested
    Designing Switchmode Transformers for Optimum Efficiency | Content content from Power Electronics starting point with What is an SMPS | Switch Mode Power Supply Tutorial | Radio-Electronics.com tutorial…
  • michaelkellett
    michaelkellett over 11 years ago +1
    I don't know if there is some material on the web (I expect that there is) but I once attended a very good TI seminar about power supplies with a very good lecture on transformer/inductor design. MK
  • kkazem
    kkazem over 11 years ago in reply to peterjcs23 +1 suggested
    Peter, Unless you need that evaluation kit for the electronic converter, I'd say away from it as It looks like it has a ready-made transformer in it. If you want to design and build your own transformer…
Parents
  • D_Hersey
    0 D_Hersey over 11 years ago

    SMPS is fascinating and at the cutting edge of linear design.  If one wants to get into it I recommend designing small supplies, in the 1 - 10 Watt regime and keeping below, say, 24V at first, and not leaving one's circuits energized and unattended at first.  There are different rules for insulation when transformers are used in higher-power regimes, and regulations to follow.  If one takes on the challenges of more sophisticated topologies, higher operating frequencies, and higher-power regimes stepwise he will benefit.  My opinion is that this isn't somewhere where one should start at the top.  It is its own discipline.

     

    Peter, you're welcome.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kkazem
    0 kkazem over 11 years ago in reply to D_Hersey

    Well, there's some mis information here. There certainly are flyback transformers and while there may be a few people calling them transductors (I've never heard the term before in my 35 years of power conversion design), the engineers in the industry call them flyback transformers. One could say that every transformer is a coupled inductor; it's not really instructive. A flyback transformer is different than most transformers in that a lot of energy is stored in the core while the main (usually) MOSFET switch is on and no power is being transferred to the secondary. When the switch is opened, the energy stored in the core is then transferred to the secondary as the polarity of the secondary voltage changes nearly instantaneously when the switch gets opened. In most flyback transformers, energy is stored in air gaps since a ferrite or other non-gapped core material cannot store much energy. SOme cores have what's called a distributed (air) gap and are made from a type of powder that has a filler between magnetic particles to provide the gap. Other's use a standard ferrite core, but with a fixed gap between where the core halves come together. This can be made by milling the center core (preferred method) or by inserting a suitable material, like Nomex between the core halves.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • kkazem
    0 kkazem over 11 years ago in reply to D_Hersey

    Well, there's some mis information here. There certainly are flyback transformers and while there may be a few people calling them transductors (I've never heard the term before in my 35 years of power conversion design), the engineers in the industry call them flyback transformers. One could say that every transformer is a coupled inductor; it's not really instructive. A flyback transformer is different than most transformers in that a lot of energy is stored in the core while the main (usually) MOSFET switch is on and no power is being transferred to the secondary. When the switch is opened, the energy stored in the core is then transferred to the secondary as the polarity of the secondary voltage changes nearly instantaneously when the switch gets opened. In most flyback transformers, energy is stored in air gaps since a ferrite or other non-gapped core material cannot store much energy. SOme cores have what's called a distributed (air) gap and are made from a type of powder that has a filler between magnetic particles to provide the gap. Other's use a standard ferrite core, but with a fixed gap between where the core halves come together. This can be made by milling the center core (preferred method) or by inserting a suitable material, like Nomex between the core halves.