Power & Energy
  • Technologies
  • More
Power & Energy
Forum dc step up circuit
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Subscribers 283 subscribers
  • Views 644 views
  • Users 0 members are here
Related

dc step up circuit

gabyhass
gabyhass over 11 years ago

I'm looking to power my old spy gear trackr with rechargeable batteries,but I need to boost a 3.6v 1200ma battery to 9v @1200ma

Its ni-mh and a ni-cd 2.4v @ 800ma to 6v @ 800ma I know that step-up circuits reduce the amount of current it outputs so how many Ma should the battery be to compensate for the reduction and could someone also help me understand boost circuits so I can create my own in the future

 

-thanks Gabriel wells

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 11 years ago +2 verified
    Hi Gabe, You can do a rough calculation of the maximum you can expect on a step up by multiplying the amps times the volts of the input and it will be equal to the amps times the volts of the output. For…
  • jw0752
    0 jw0752 over 11 years ago

    Hi Gabe,

    You can do a rough calculation of the maximum you can expect on a step up by multiplying the amps times the volts of the input and it will be equal to the amps times the volts of the output. For example if you have 3.6v and 1200mA ( which is 1.2A) then we get 3.6V X 1.2A = 4.32VA  If we step up to 9volts we just divide 4.32VA by the 9 volts and get .48A or in other words 480mA. In real life there is always some loss in the change over so these numbers are going to be too high. Perhaps we might realistically expect to get 9 volts 400mA.

     

    Here is a link to a circuit that can perhaps make the boost that you are looking for. If not there are many different ones listed too.

     

    http://www.ebay.com/itm/DC-DC-Adjustable-Step-up-boost-Power-Converter-Module-XL6009-Replace-LM2577-/181608388242?pt=LH_DefaultDomain_0&hash=item2a48b41692

     

    I would check the internet for information on switching and boost circuits if you want more information on how they are designed as it isn't simple.

     

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • element14support
    0 element14support over 11 years ago

    Hello gabyhass

    Welcome to the element14 Community, I will move this over to the Power Management area as it is a better fit.

     

    Thank you,

     

    Jamie

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago

    element14jamie - Hi Jamie, this thread was another one where several days ago I replied via email and it did not get inserted. Hope it can help with diagnosis

    Thanks

    Peter