Power & Energy
  • Technologies
  • More
Power & Energy
Forum MOSFET Gate Driver with Isolated Logic Ground
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 283 subscribers
  • Views 1114 views
  • Users 0 members are here
  • mosfet
  • inverter
  • mosfet_drivers
  • power_electronics
Related

MOSFET Gate Driver with Isolated Logic Ground

e14 Contributor
e14 Contributor over 11 years ago

Hi,

 

I'm designing a board with a single phase inverter, three phase inverter and a buck-boost DC-DC converter (all driven with MOSFETS).

 

I need to keep the power nets separate from the logic/signal nets.

 

I've found a high side driver for DC-DC converter. This is suitable for the application as it doesn't assume common grounds.

 

I would like to use half-bridge MOSFET drivers for the two inverters (i.e. five in total), unless there are suitable full-bridge and 3ph ICs available.

 

However... I can't find a suitable IC because they all seem to assume common ground on the low side (i.e. connecting the source of the MOSFET with logic ground). I want to keep the logic/signal ground net separate from the power nets.


Question:

Are there any ICs out there that do not connect the low side source to logic ground? (1ph and 3ph, OR half-bridge)

 

Specs:

This isn't a high voltage application. The power nets have limits of (-25V, +25V) and (-5A, +5A)

 

As for logic and signals: logic is 5V; and power supplies rails are +5V, -15V, +15V and GND.

 

Thanks for your help!

  • Sign in to reply
  • Cancel
Parents
  • clem57
    0 clem57 over 11 years ago

    I am not sure of why you want this, but I see H-Bridge Modified Sine Wave Inverter Circuit | Homemade Circuit Projects.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 11 years ago

    I am not sure of why you want this, but I see H-Bridge Modified Sine Wave Inverter Circuit | Homemade Circuit Projects.

    Clem