Power & Energy
  • Technologies
  • More
Power & Energy
Forum Power use of transformers, dependent on load?
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 8 replies
  • Answers 6 answers
  • Subscribers 288 subscribers
  • Views 6567 views
  • Users 0 members are here
  • transformer
  • power
Related

Power use of transformers, dependent on load?

ntewinkel
ntewinkel over 11 years ago

Hi all,

 

I'm wondering if the power used by a transformer varies depending on the load put on the transformer.

 

The specific situation is my 12 volt landscape/deck lighting - I have a transformer on the wall rated to supply a maximum of 120 watts. I recently upgraded to LED lights to replace the old 7 watt bulbs.

 

Does the transformer now use less power from my house wiring, now that I have LED bulbs that draw less power on the output side?

 

The reason for the question is that I'm wondering if it would make sense to replace the big transformer with a smaller transformer.

I recall the electric company going on about wall chargers always consuming power even when it they are not charging any device.

 

ps, I plugged in a power meter (left over from my days as residential energy advisor), on the 120v side, and measured that the transformer now uses about 0.20 amps (= 24 watts?).

 

Thanks!

-Nico

  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 11 years ago in reply to johnbeetem +3 suggested
    John is pretty close .... A wall wart tends to have a DC to DC converter, with capacitors and maybe a regulator, so it will consume some power while there is no load. More importantly the capacitors will…
  • ntewinkel
    ntewinkel over 11 years ago in reply to clem57 +2 suggested
    2.4 watts would be excellent, but that tester was plugged in on the 120 volt side, which makes it 24 watts then? - still good for the 8 LED lights (3 watts each average).
  • johnbeetem
    johnbeetem over 11 years ago +2 suggested
    Nico wrote: I'm wondering if the power used by a transformer varies depending on the load put on the transformer. I would say yes, definitely. If you feel a wall wart that's plugged into the wall but…
Parents
  • kkazem
    0 kkazem over 6 years ago

    Yes, the power used by (not transferred out of) a transformer increases with load.

    1. The magnetic losses, due to magnetizing the core does not change with load, only with input voltage (increasing) and with input frequency (increasing).

     

    2. The copper losses increase with load. This goes for both the primary and the secondary winding losses.

     

    Absolutely, decreasing the lamp wattage load on your transformer reduces both the primary and secondary current. Since the primary and secondary winding resistances are fixed (at any given temperature), the (I^2)*R losses will be less by the square of the reduced current.  

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • kkazem
    0 kkazem over 6 years ago

    Yes, the power used by (not transferred out of) a transformer increases with load.

    1. The magnetic losses, due to magnetizing the core does not change with load, only with input voltage (increasing) and with input frequency (increasing).

     

    2. The copper losses increase with load. This goes for both the primary and the secondary winding losses.

     

    Absolutely, decreasing the lamp wattage load on your transformer reduces both the primary and secondary current. Since the primary and secondary winding resistances are fixed (at any given temperature), the (I^2)*R losses will be less by the square of the reduced current.  

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer