Power & Energy
  • Technologies
  • More
Power & Energy
Forum Inaccurate Readings from Thermal Imaging Camera on Copper Heatsink-Anyone Else Had this Happen?
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 6 replies
  • Answers 1 answer
  • Subscribers 281 subscribers
  • Views 10223 views
  • Users 0 members are here
  • dc-dc
  • Design
  • power_supply
Related

Inaccurate Readings from Thermal Imaging Camera on Copper Heatsink-Anyone Else Had this Happen?

kkazem
kkazem over 4 years ago

I have a Fluke Ti25 Thermal Imaging Camera that I used on a 1,200 watt PFC Controller to measure the power FET and power diode temps. The Fluke camera has an adjustment for emissivity, which I set to copper (I don't recall the value). I chose this as my heatsink was a copper bar. Using both my finger (with the power off, of course) and a thermocouple, I'm confident the actual temperature was about 85 Celsius, but the Fluke IR camera said it was 15 Celsius. Clearly, this reading was wrong as my lab is in Southern California and it was done in late summer. The temperature never gets below 70 F (21.1 C) and this heat sink was hot to the touch. 

The literature says it may be due to reflected energy instead of emitted energy. So I changed the angle of the camera with respect to the heatsink and it didn't make much difference. The literature also says to put black tape on the surface or to paint it black, but both of those would be problematic on my heat sink as it would interfere with convection cooling off of the copper bar heat sink. The devices were TO-247 (one FET and one SiC Diode) on a 4" x 1" x 0.19" thick copper bar. The devices were mounted with a 6-32 screw and nut and tightened appropriately. 

Has anyone else had similar problems and if so, do you have any tips on how to correct it to obtain more accurate temperature values from the IR camera?

image

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 4 years ago +6
    In some cases I have bolted on a piece of black anodized aluminum to make non-contact thermal measurements. This also increased the surface area which helped my device stay cooler. I happen to have a stack…
  • Gough Lui
    Gough Lui over 4 years ago +6
    An infrared camera measures the long-wave infrared light emitted by a hot object and does not measure temperature directly. It converts the measured amount of infrared to a temperature by assuming a value…
  • cheetat
    cheetat over 4 years ago +6 suggested
    The copper plate in the photo appears to be commercial burnished and it may have low emissivity value (0.07). This maybe a value to start with if you are doing a rough measurement. https://www.ntnu.no…
Parents
  • cheetat
    0 cheetat over 4 years ago

    The copper plate in the photo appears to be commercial burnished and it may have low emissivity value (0.07). This maybe a value to start with if you are doing a rough measurement.

    https://www.ntnu.no/wiki/display/digilab/Fluke+TiR32+Thermal+Imager?preview=/67469543/67567689/3038318_A_w.jpg

    Correct emissivity value is important to determine the measured temperature of a target that you are working on. If you are not comfortable working with painting the copper plate in black, try to use electrical tape (most of them would have emissivity value between 0.95 - 0.97). 3M Scotch 88 Vinyl electrical tape has emissivity value of 0.96 (this should be the emissivity that you set initially) and you may temporary stick a piece of the tape on the copper tape to measure the temperature of the copper plate, record the temperature and remove the tape from the copper plate. Ti25 offer on-screen emissivity correction so after removing the tape, you may adjust the emissivity value to the same temperature value that you have recorded earlier and you should obtain the correct temperature reading with the correct emissivity value moving onwards. Measuring with another measurement source such as thermocouple as a temperature reference works as well (just that it may be a more expensive solution to work on).

    More readings on emissivity for thermal imager - https://www.flir.com/discover/rd-science/use-low-cost-materials-to-increase-target-emissivity/ 

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • cheetat
    0 cheetat over 4 years ago

    The copper plate in the photo appears to be commercial burnished and it may have low emissivity value (0.07). This maybe a value to start with if you are doing a rough measurement.

    https://www.ntnu.no/wiki/display/digilab/Fluke+TiR32+Thermal+Imager?preview=/67469543/67567689/3038318_A_w.jpg

    Correct emissivity value is important to determine the measured temperature of a target that you are working on. If you are not comfortable working with painting the copper plate in black, try to use electrical tape (most of them would have emissivity value between 0.95 - 0.97). 3M Scotch 88 Vinyl electrical tape has emissivity value of 0.96 (this should be the emissivity that you set initially) and you may temporary stick a piece of the tape on the copper tape to measure the temperature of the copper plate, record the temperature and remove the tape from the copper plate. Ti25 offer on-screen emissivity correction so after removing the tape, you may adjust the emissivity value to the same temperature value that you have recorded earlier and you should obtain the correct temperature reading with the correct emissivity value moving onwards. Measuring with another measurement source such as thermocouple as a temperature reference works as well (just that it may be a more expensive solution to work on).

    More readings on emissivity for thermal imager - https://www.flir.com/discover/rd-science/use-low-cost-materials-to-increase-target-emissivity/ 

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer