Power & Energy
  • Technologies
  • More
Power & Energy
Forum purpose of Schottky diode in the circuit
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 6 replies
  • Subscribers 280 subscribers
  • Views 4620 views
  • Users 0 members are here
Related

purpose of Schottky diode in the circuit

ravi kondeti
ravi kondeti over 4 years ago

Hello 

i came across a circuit as shown below. here 20 volt battery is used as source. microcontroller is used to switch the NMOS. i am not able to understand the use of the diode placed across the gate and source of the PMOS. can anyone explain?

Thank you 

image

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 4 years ago +3 verified
    Hello, (Replying from mobile so will be brief) I think this circuit is a mess, better to look for a more appropriate one, it has quite a few flaws. Anyway it is more likely a Zener diode even though…
  • ravi kondeti
    ravi kondeti over 4 years ago in reply to shabaz +1
    hello shabaz.yes its a zener, thank you for the correction. my doubt is when supply voltage is a battery, assuming NMOS is on, even though battery is increased from 20 to 60 volts. voltage across gate…
  • dougw
    dougw over 4 years ago in reply to ravi kondeti +1 verified
    If the voltage divider is calculated to handle both high and low battery voltage extremes and circuit switching speed requirements, then the zener is just for insurance. The battery won't have transients…
Parents
  • shabaz
    +1 shabaz over 4 years ago

    Hello, 

    (Replying from mobile so will be brief)

    I think this circuit is a mess, better to look for a more appropriate one, it has quite a few flaws. Anyway it is more likely a Zener diode even though it says Schottky, and I'm guessing it was an attempt to protect the gate of the P-ch MOSFET since it may only be rated to say 20V or less, and the supply voltage could easily be higher. Also since you have it in a simulation package (looks like TINA simulator?) you could simulate this.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • ravi kondeti
    0 ravi kondeti over 4 years ago in reply to shabaz

    hello shabaz.yes its a zener, thank you for the correction. my doubt is when supply voltage is a battery, assuming NMOS is on, even though battery is increased from 20 to 60 volts. voltage across gate and source will not be crossing over 20 volts due to the voltage divider. is it correct scenario or should i consider higher voltage transients? 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dougw
    +1 dougw over 4 years ago in reply to ravi kondeti

    If the voltage divider is calculated to handle both high and low battery voltage extremes and circuit switching speed requirements, then the zener is just for insurance.

    The battery won't have transients but it can be a bit higher than its nominal rated value.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • dougw
    +1 dougw over 4 years ago in reply to ravi kondeti

    If the voltage divider is calculated to handle both high and low battery voltage extremes and circuit switching speed requirements, then the zener is just for insurance.

    The battery won't have transients but it can be a bit higher than its nominal rated value.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • ravi kondeti
    0 ravi kondeti over 4 years ago in reply to dougw

    hello dougw, that seems about right. thank you