Power & Energy
  • Technologies
  • More
Power & Energy
Forum lipo battery charging directly with solar panel
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Subscribers 280 subscribers
  • Views 10661 views
  • Users 0 members are here
Related

lipo battery charging directly with solar panel

ravi kondeti
ravi kondeti over 4 years ago

Hello,

I am building a solar battery module for LED lighting application. Task here was to use least hardware possible to reduce the cost per board. I read online that a solar panel with less than 5 watts can be used without a charger circuit. my battery is 

also a smaller one with 7.4 volts. panels outs 12 volts, < 5watts. can I keep a resistor in between them and a diode in series for unidirectional current flow? will it be sufficient for general purpose use?

  • Sign in to reply
  • Cancel

Top Replies

  • MK.Mcleary
    MK.Mcleary over 4 years ago +4 verified
    A lithium ion battery should never be changed without overcharge protection. Some batteries have a built in protection board. This prevents overcharge and overdischarge. In case there is such a built…
  • vishnu_n93
    vishnu_n93 over 4 years ago +3 verified
    A diode would only help you to control the direction of current flow, and ensure that your batteries do not get drained through the solar panel. However It does not provide overvoltage protection for your…
  • kkazem
    kkazem over 4 years ago +3 verified
    Even though only 5W, I would recommend to charge the battery thru a 3-terminal linear regulator if you want maximum simplicity. You'll need to know the fully charged voltage and can use either an adjustable…
Parents
  • vishnu_n93
    +1 vishnu_n93 over 4 years ago

    A diode would only help you to control the direction of current flow, and ensure that your batteries do not get drained through the solar panel.
    However It does not provide overvoltage protection for your batteries. Depending on the voltage and curret profile of your solar panel, the battery may initially charge without any issues as long as the voltage stays below 7.4V as you draw current. But as your battery voltage approaches 7.4, and the solar panel is capable of providing upto 12V (or actually more depending on sunlight), the voltage would now rise, thereby damaging your batteries.

    The cheapest solution would be to put a zener of 7.4V and high enough power (>5W in this case) parallel to your solar panel, and then continue with the series diode and resistor approach.
    Even though this solution is not perfect, it should solve your problem.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • vishnu_n93
    +1 vishnu_n93 over 4 years ago

    A diode would only help you to control the direction of current flow, and ensure that your batteries do not get drained through the solar panel.
    However It does not provide overvoltage protection for your batteries. Depending on the voltage and curret profile of your solar panel, the battery may initially charge without any issues as long as the voltage stays below 7.4V as you draw current. But as your battery voltage approaches 7.4, and the solar panel is capable of providing upto 12V (or actually more depending on sunlight), the voltage would now rise, thereby damaging your batteries.

    The cheapest solution would be to put a zener of 7.4V and high enough power (>5W in this case) parallel to your solar panel, and then continue with the series diode and resistor approach.
    Even though this solution is not perfect, it should solve your problem.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • ravi kondeti
    0 ravi kondeti over 4 years ago in reply to vishnu_n93

    interesting approach. i kept a MOSFET on off control for over voltage protection. this seems simpler and reducing more no of components. thank you