Power & Energy
  • Technologies
  • More
Power & Energy
Forum MOSFET going to continuous conduction
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 17 replies
  • Subscribers 278 subscribers
  • Views 13578 views
  • Users 0 members are here
Related

MOSFET going to continuous conduction

ravi kondeti
ravi kondeti over 4 years ago

Hello Guys,

Following is a circuit i am working on. input is from a isolated DC-DC converter (flyback configuration) set at 12v. using bk precision electronic load i am testing at 500mA. i wanted to observe the dynamic behaviour of flyback converter while switching the load at higher rate so i kept a mosfet rated for 60V,2A. while switching observed that current is peaking and FET is gone. later changed FET to a higher rating one (TK4R1A10PL). even then MOSFET after sometime goes into continuous conduction even when i am removing gate pulses (using a function generator to give pulses), this is happening when i am increasing the frequency of the gate pulses (5-10kHz). using function generator a wrong approach? or any corrections i need make. please suggest

image

  • Sign in to reply
  • Cancel

Top Replies

  • navadeepganeshu
    navadeepganeshu over 4 years ago +7
    Hi Ravi, The 60V, 2A MOSFET seems ok for this application. But just ensure that the MOSFET is able to drive that much current for the gate voltage you apply(the Vgs/Id characteristics in the datasheet…
  • shabaz
    shabaz over 4 years ago +6
    Hi, Continuous conduction means the MOSFET is damaged, one or more parameters was exceeded. To troubleshoot, you'd need a 'scope probe to see the gate voltage and the drain with respect to the source…
  • dougw
    dougw over 4 years ago +6
    A FET in this configuration would likely only die from heat. If the device didn't get hot to the touch it means it would have been a very fast internal heating due to high inrush current. If it did get…
Parents
  • shabaz
    0 shabaz over 4 years ago

    Hi,

    Continuous conduction means the MOSFET is damaged, one or more parameters was exceeded. To troubleshoot, you'd need a 'scope probe to see the gate voltage and the drain with respect to the source. It could be as simple as needing a 50 ohm resistor wired between the gate and source (otherwise the gate sees a signal which is different from what you have configured on the function generator, but you won't know that without looking at it with a 'scope). Also it will be noticeable at high frequencies that the function generator impedance might not charge/discharge the MOSFET gate fast enough. Also, long wires will act as inductors, causing voltage spikes when the MOSFET switches off. There are techniques to eliminate that, you could try a ferrite beads.. but really you're flying blind without looking at it. Before the MOSFET blows, start at a lower voltage or frequency and record the signals from your 'scope, and actually see what is causing it.

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ravi kondeti
    0 ravi kondeti over 4 years ago in reply to shabaz

    hello shabaz,

    i was observing the current through the MOSFET and voltage output of the flyback converter. there is a current spike of 8 times the set load current. unfortunately i was not able to save those plots as i was not sure what was happening in the moment. i will repeat the test with a plain R load and shorter leads and try to check on the parameters properly. i will try to replace the function generator with a proper gate driver and check again.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ravi kondeti
    0 ravi kondeti over 4 years ago in reply to shabaz

    hello shabaz,

    i was observing the current through the MOSFET and voltage output of the flyback converter. there is a current spike of 8 times the set load current. unfortunately i was not able to save those plots as i was not sure what was happening in the moment. i will repeat the test with a plain R load and shorter leads and try to check on the parameters properly. i will try to replace the function generator with a proper gate driver and check again.