Power & Energy
  • Technologies
  • More
Power & Energy
Forum MOSFET going to continuous conduction
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 17 replies
  • Subscribers 278 subscribers
  • Views 13566 views
  • Users 0 members are here
Related

MOSFET going to continuous conduction

ravi kondeti
ravi kondeti over 4 years ago

Hello Guys,

Following is a circuit i am working on. input is from a isolated DC-DC converter (flyback configuration) set at 12v. using bk precision electronic load i am testing at 500mA. i wanted to observe the dynamic behaviour of flyback converter while switching the load at higher rate so i kept a mosfet rated for 60V,2A. while switching observed that current is peaking and FET is gone. later changed FET to a higher rating one (TK4R1A10PL). even then MOSFET after sometime goes into continuous conduction even when i am removing gate pulses (using a function generator to give pulses), this is happening when i am increasing the frequency of the gate pulses (5-10kHz). using function generator a wrong approach? or any corrections i need make. please suggest

image

  • Sign in to reply
  • Cancel

Top Replies

  • navadeepganeshu
    navadeepganeshu over 4 years ago +7
    Hi Ravi, The 60V, 2A MOSFET seems ok for this application. But just ensure that the MOSFET is able to drive that much current for the gate voltage you apply(the Vgs/Id characteristics in the datasheet…
  • shabaz
    shabaz over 4 years ago +6
    Hi, Continuous conduction means the MOSFET is damaged, one or more parameters was exceeded. To troubleshoot, you'd need a 'scope probe to see the gate voltage and the drain with respect to the source…
  • dougw
    dougw over 4 years ago +6
    A FET in this configuration would likely only die from heat. If the device didn't get hot to the touch it means it would have been a very fast internal heating due to high inrush current. If it did get…
Parents
  • dougw
    0 dougw over 4 years ago

    A FET in this configuration would likely only die from heat. If the device didn't get hot to the touch it means it would have been a very fast internal heating due to high inrush current.

    If it did get hot, then maybe the drive signal isn't turning the FET on completely. What gate voltage is being used?

    Is it possible to measure the transient current during turn on of the load?

    One other possibility is if the load is inductive there could be a high voltage spike on turn off. This could be mitigated using a snubber diode across the load. 

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ravi kondeti
    0 ravi kondeti over 4 years ago in reply to dougw

    hello dougw,

    i was observing a peaking current while turn on nearly 8 times the set point(500mA). i observed that initially heating was occuring so chose a fet with higher power rating. i am using a function generator with 10V amplitude.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dougw
    0 dougw over 4 years ago in reply to ravi kondeti

    It should be very tough to kill the big Toshiba FET, although it may need a heatsink if it is getting too hot to touch. Is it possible it is just connected incorrectly (drain and source swapped) and the body diode is conducting?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • dougw
    0 dougw over 4 years ago in reply to ravi kondeti

    It should be very tough to kill the big Toshiba FET, although it may need a heatsink if it is getting too hot to touch. Is it possible it is just connected incorrectly (drain and source swapped) and the body diode is conducting?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • ravi kondeti
    0 ravi kondeti over 4 years ago in reply to dougw

    Connection was fine, as I checked at lower frequency switching is happening.