Power & Energy
  • Technologies
  • More
Power & Energy
Forum MOSFET going to continuous conduction
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 17 replies
  • Subscribers 280 subscribers
  • Views 13454 views
  • Users 0 members are here
Related

MOSFET going to continuous conduction

ravi kondeti
ravi kondeti over 4 years ago

Hello Guys,

Following is a circuit i am working on. input is from a isolated DC-DC converter (flyback configuration) set at 12v. using bk precision electronic load i am testing at 500mA. i wanted to observe the dynamic behaviour of flyback converter while switching the load at higher rate so i kept a mosfet rated for 60V,2A. while switching observed that current is peaking and FET is gone. later changed FET to a higher rating one (TK4R1A10PL). even then MOSFET after sometime goes into continuous conduction even when i am removing gate pulses (using a function generator to give pulses), this is happening when i am increasing the frequency of the gate pulses (5-10kHz). using function generator a wrong approach? or any corrections i need make. please suggest

image

  • Sign in to reply
  • Cancel

Top Replies

  • navadeepganeshu
    navadeepganeshu over 4 years ago +7
    Hi Ravi, The 60V, 2A MOSFET seems ok for this application. But just ensure that the MOSFET is able to drive that much current for the gate voltage you apply(the Vgs/Id characteristics in the datasheet…
  • shabaz
    shabaz over 4 years ago +6
    Hi, Continuous conduction means the MOSFET is damaged, one or more parameters was exceeded. To troubleshoot, you'd need a 'scope probe to see the gate voltage and the drain with respect to the source…
  • dougw
    dougw over 4 years ago +6
    A FET in this configuration would likely only die from heat. If the device didn't get hot to the touch it means it would have been a very fast internal heating due to high inrush current. If it did get…
Parents
  • scottiebabe
    0 scottiebabe over 4 years ago

    With a DSO, you don't really need a high repetition rate to measure step response. If you are burning out FETs start with a slower switching frequency of say 10 -100 Hz. 

    If you add some series resistance to the drain of T1, you will see the electronic load doesn't really behave as a great current source at high frequencies. 

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ravi kondeti
    0 ravi kondeti over 4 years ago in reply to scottiebabe

    I will be Replacing the electronic load with a resistor. Does it seems to be ok for higher switching rates? 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kkazem
    0 kkazem over 4 years ago in reply to ravi kondeti

    In general, yes. But if you want it to handle high rate of rise of current/voltage, then do not use an inductive resistor, the best type is a carbon comp or a metal film or metal oxide for low inductance, You can combine many smaller ones to make a larger power handling ability. Also, any wiring between your source and load should have twisted pair wiring or coaxial wiring, again, to minimize inductance.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • kkazem
    0 kkazem over 4 years ago in reply to ravi kondeti

    In general, yes. But if you want it to handle high rate of rise of current/voltage, then do not use an inductive resistor, the best type is a carbon comp or a metal film or metal oxide for low inductance, You can combine many smaller ones to make a larger power handling ability. Also, any wiring between your source and load should have twisted pair wiring or coaxial wiring, again, to minimize inductance.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • ravi kondeti
    0 ravi kondeti over 4 years ago in reply to kkazem

    Hi kkazem, 

    I will note these. Thank you