Power & Energy
  • Technologies
  • More
Power & Energy
Forum IKEA filament type LED buld - unveal the individual LEDs
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 279 subscribers
  • Views 1687 views
  • Users 0 members are here
Related

IKEA filament type LED buld - unveal the individual LEDs

Jan Cumps
Jan Cumps over 4 years ago

I bought a TRÅDFRI LED lamp a while ago. It's the type that looks like a traditional lamp, with a filament.

image

image: IKEA

When you look at the lamp (switched on or off) you can't see the individual LEDs. But the fumed glass lampshade that I have put it in, reflects the light, and you can see the individual little LEDs in the reflection with the naked eye:

image

I took the photo with the lowest possible exposure. Here's normal exposure:

image

As usual, the photo does not show what I really see :). So hard to photograph light and achieve the actual WYSIWYG.

  • Sign in to reply
  • Cancel

Top Replies

  • Gough Lui
    Gough Lui over 4 years ago +3
    Some bulbs can be dimmed, which would make spotting them easier ... I've only got linear filament bulbs - e.g. https://goughlui.com/2022/09/04/quick-review-lenovo-smart-filament-bulb-g95-e27-806lm-se…
  • genebren
    genebren over 4 years ago +2
    LED filaments are being used a lot these days. I have found that if I take control of the intensity range on my phone, I can capture an image the is not saturated on the highest intensity. Then I can use…
  • shabaz
    shabaz over 4 years ago +1
    LED filaments are cool : ) Some look better than traditional tungsten looked like : ) Interesting how the shade reflection helped with the photo. Maybe there's some polarization or something going on…
Parents
  • genebren
    genebren over 4 years ago

    LED filaments are being used a lot these days.  I have found that if I take control of the intensity range on my phone, I can capture an image the is not saturated on the highest intensity.  Then I can use an image processor package (I use ImageJ) to threshold the the image and create a visible separation between the bright pixel, enough to expose the slight gaps in the LED filament.

    Still, cool light and fixture.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • genebren
    genebren over 4 years ago

    LED filaments are being used a lot these days.  I have found that if I take control of the intensity range on my phone, I can capture an image the is not saturated on the highest intensity.  Then I can use an image processor package (I use ImageJ) to threshold the the image and create a visible separation between the bright pixel, enough to expose the slight gaps in the LED filament.

    Still, cool light and fixture.