Power & Energy
  • Technologies
  • More
Power & Energy
Forum Power banks for Home IT equipment - anyone used them?
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 30 replies
  • Subscribers 281 subscribers
  • Views 6796 views
  • Users 0 members are here
  • backup supply
  • power bank
Related

Power banks for Home IT equipment - anyone used them?

shabaz
shabaz over 4 years ago

Several friends have been discussing the need to be prepared when/if there are power outages in the UK in Winter or Spring.

Our assumption is that the outage would not be longer than a day. Some of the battery backup systems cost thousands, which could be justified (say) over a 5-year life period, but it's unrealistic in the UK to want to be prepared with a backup source for 5 years for the home, given that any power outages won't be very frequent. Granted that backup systems could be used to obtain cheap(er) electricity at off-peak times, but it is hard to predict if the savings will be that significant enough to justify the big up-front expense commitment.

A generator is unattractive because of the noise, but we are open to it, but would definitely prefer a battery solution. Cooking food with an electricity source isn't too important; if there isn't natural gas connection in the kitchen, then camping gear could be used.

Then we noticed there are power banks. Some are in the $200 price range, many are $300-$500, and there are others circa $1000 and beyond.

There are lots of obscure power bank products such as the one below. It's a lot of energy to keep in a home, so whatever is used needs to be safe.

image (Image source: Amazon)

Backup lighting sources are cheap; there are even power tool ecosystems that use the same battery for task lights, so they could be used in a pinch. Not elegant, but it gets the job done at low cost.

However, we were not sure how to deal with IT equipment. Routers/DSL modems are straightforward because they operate from 12V or 5V and a backup supply is easily rigged up for that.

For laptops, it could be attractive to have a backup supply that offers USB Type C output, since many laptops (or lower power chromebooks) have a USB-C socket for power nowadays.

Any battery banks, or other backup scheme, that people can recommend? It would be nice to be able to charge (and run) laptops and power and charge anything that uses a USB connector. Perhaps a minimum of 100W power support would be needed, although really several hundred W would be preferred, so that a couple of laptops could be run, iPad, phones charged and so on. An additional 12V output would be a nice-to-have, to charge up or operate other devices. AC mains output is not essential. Hot-standby is not essential either, since a laptop will continue to run on its own battery while power connections are swapped. 

Any comments/ideas appreciated!

  • Sign in to reply
  • Cancel

Top Replies

  • rsjawale24
    rsjawale24 over 4 years ago +4
    I have fibre optic broadband at home. When it was first installed around 6 years back, I was surprised to see that the ONT had it's own 12V 6Ah battery supply for power outages. The power supply is quite…
  • three-phase
    three-phase over 4 years ago +4
    I use a 500wh portable station from Power Oak. I have had it a few years now and have not had any issues with it. I use it a lot on sites for powering test apparatus when there is no power close by. I…
  • vishwasn
    vishwasn over 4 years ago in reply to shabaz +4
    As a DIY solution to the WiFi router backup issue, I made this scalable battery bank using the 18650 cells and a BMS. Since required voltage is 12V. It is easy to have 3S balancer directly connected to…
Parents
  • beacon_dave
    0 beacon_dave over 4 years ago

    "...Our assumption is that the outage would not be longer than a day..."

    You might want to rethink that bit. Slight smile

    Ever since 'Storm Desmond' took the local substation out (without power for 4 days), I've been interested in some sort of off-grid solution. More recent storms have affected other areas in a similar manner. The emergency response wasn't and hasn't been that great and you are on your own as pretty much everything instantly shuts down around you due to modern overreliance on grid power. 

    The problem with the power banks is it's hard to tell how serviceable/reliable they are. I would prefer to have something that used standard readily available batteries and that charged and monitored them in a safe manner. Ideally with a provision for solar hookup so that you can make the most of the few daylight hours when available. 

    My other thoughts were to have a small LPG generator as some of these are very quiet, and bottled gas stores quite well. Enough to keep the fridge/freezer and boiler pump powered and to charge a few batteries. LPG can be used with camping stoves/heaters as well.

    It's going to get worse here soon when they switch the analogue PSTN service off in favour of VOIP as for many that will mean no phones as well as no power. From the last outage, it doesn't appear that the mobile phone infrastructure has the same backup power that the telephone exchanges currently have. 

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • beacon_dave
    0 beacon_dave over 4 years ago

    "...Our assumption is that the outage would not be longer than a day..."

    You might want to rethink that bit. Slight smile

    Ever since 'Storm Desmond' took the local substation out (without power for 4 days), I've been interested in some sort of off-grid solution. More recent storms have affected other areas in a similar manner. The emergency response wasn't and hasn't been that great and you are on your own as pretty much everything instantly shuts down around you due to modern overreliance on grid power. 

    The problem with the power banks is it's hard to tell how serviceable/reliable they are. I would prefer to have something that used standard readily available batteries and that charged and monitored them in a safe manner. Ideally with a provision for solar hookup so that you can make the most of the few daylight hours when available. 

    My other thoughts were to have a small LPG generator as some of these are very quiet, and bottled gas stores quite well. Enough to keep the fridge/freezer and boiler pump powered and to charge a few batteries. LPG can be used with camping stoves/heaters as well.

    It's going to get worse here soon when they switch the analogue PSTN service off in favour of VOIP as for many that will mean no phones as well as no power. From the last outage, it doesn't appear that the mobile phone infrastructure has the same backup power that the telephone exchanges currently have. 

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • shabaz
    0 shabaz over 4 years ago in reply to beacon_dave

    Hi Dave,

    Wow - yes, a 4-day outage was not something that we considered! : ) I hope the electricity firm compensated financially, but I guess it's minimal. I struggled to get any compensation even though I proved the voltage was out of limits after an outage, and it destroyed some LED lights.

     By the way, there are currently some scam firms online offering low-cost generators (like £100-£150 cheaper than expected). A friend got burned by one called "gar store . co. uk", Definitely worth checking Trustpilot etc before purchasing. 

    If I could find some ready-made USB-C PD boards that would accept 12 or 24V and output 90W or so, then a lead acid battery solution could be interesting. Cheap, and reliable even though it is large. It could be stored outside, in a garden storage box, removing some of the risk of storing so much energy indoors.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 4 years ago in reply to shabaz
    shabaz said:
    If I could find some ready-made USB-C PD boards that would accept 12 or 24V and output 90W or so

    This will do 11-17V and output 60W+18W:

    https://www.hawkwoods.co.uk/Cine/P/I-PWC

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 4 years ago in reply to shabaz
    shabaz said:
    The past few times an outage occurred, the phone lines worked, since BT legally are not allowed more than a 6-minute outage as far as I understand (otherwise they have to report to the government) however I can't recall if that extended to DSL, it might just be for voice. I have a spare 4G/LTE modem so worst case I can get that going, it just requires a 5V DC source. Definitely a good idea to have a normal phone at home too, and not just cordless.

    I think that is all about to change after 2025 with the removal of the PSTN service. Originally Ofcom were suggesting that telecoms providers had to provide a backup power solution for the DSL router for VOIP during a power outage, however that appears to have been downplayed to vulnerable people only.

    I noticed that BT were suggesting that you now have a mobile for emergency use and that mobile providers suggest that you have a landline for emergency use... Anyone else see a problem here? 

    Your 4G/LTE modem won't be of much use when the mobile cells go out along with the power.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 4 years ago in reply to shabaz
    shabaz said:
    then a lead acid battery solution could be interesting. Cheap, and reliable even though it is large

    Ironically my lead acid battery backup + inverter solution failed during the storm. I think my solar trickle charger had possibly been gassing it.

    However, I've not had a great success with batteries in general. About 20 out of 25 of the UPS solutions I have worked with, have all failed within a very short space of time. Some didn't even make it through their warranty period.

    The trouble is they tend not to give any indication of a problem. They tend to pass the short self-test but then when you need them to deliver, they fail in use well before their rated capacity. 

    I was wondering if any of the standard LiFePO4 packs proved to be any more reliable. The other side of it is the battery management and charging modules.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 4 years ago in reply to beacon_dave

    Ah, just saw your comment. That looks about right, just the sort of product to DIY up a solution. The price is pretty reasonable too (£125), worth that for reliability/safety.

    I had a look on AliExpress earlier today, and ordered this (mainly because I saw a teardown on the Internet of another model by the same manufacturer, and it looked good, so I'm hoping this one might be too):

    image

    While I was at it, I also ordered the following unknown board, since it was cheap and worth a shot trying out too (both of these with a dummy load, not laptop!):

    image

    My laptop struggles to charge on 90W USB PD, but I could disable features/dim display, or use Chromebook/iPad etc, if things get difficult.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 4 years ago in reply to beacon_dave

    Why am I not surprised : ) Ofcom are useless : ) A bit like Ofwat, more in it to serve the industry rather than the consumers. If only they could get rid of the customers, all their problems would be solved : )