Power & Energy
  • Technologies
  • More
Power & Energy
Forum LED Worklight and teardown
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 26 replies
  • Subscribers 280 subscribers
  • Views 6294 views
  • Users 0 members are here
  • robogary
  • power_supply
  • power_conversion
Related

LED Worklight and teardown

robogary
robogary over 2 years ago

My workshop areas have eight 4 foot double tube fluorescent worklights in the man-cave. I installed the 4 foot floursecent fixtures 35 years ago. 

As the tubes fail,  they get consolidated, and one by one empty fluorescent fixtures get replaced with LED worklights. 5 of 8 fluorescents are still in service.

One of the LED worklights failed after a couple years of service. The failure is weird, the worklight had turned into a strobe light. 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Maybe the light can be repaired ?

I dunno, but the opportunity to troubleshoot, reverse engineer,  and maybe even scavenge parts is too good an opportunity to pass up. 

The endcaps are removed from the light fixture. The simplicity is smart. An extruded aluminum tube body, diffuser slides into it, and an LED strip is mounted on the AL extrusion.

image

The power supply leads were desoldered and the LED strip slide right out.  

The LED strip is on a thin fiberglas pcb with 78 COB LED packages soldered in place.The LED strip is labeled with 94v. 

Its easy to follow the traces to see the LED strip has 3 parallel circuits of 26 COB LEDS in series. 

image

Since the LED fixture was strobing, the LEDs seem OK, but the power supply would collapse after being able to start. 

The power supply was tucked inside the aluminum extrusion, encased in an insulated tube.

image

The power supply was first inspected for failed components. The parts are really packed in there. 

Voila !  Nothing smoked. That black thing looks like its had an overtemp near the body. Its labeled L1, ah...an inductor. 

After desoldering and removing, a closer look seems that the inductor had bitty wire leads soldered onto the stiffer component leads.

Ohm check shows its not dead shorted, and LCR meter sez its 1.86 mH. Darn, that seems reasonable. 

The inductor probably isn't bad so it will have to be reinstalled onto the power supply card.

image

Next step is to do reverse engineering on the power supply card to identify components. 

Its for sure a 120VAC 60 Hz to ~ 80Vdc (?) switching power supply, and appears to have 2 stages.  I'll need to surf for info on switching power supply basics.

 If anyone who has alot of design or service experience on switching power supplies, it would be appreciated to share some insights and hints  :-) 

  • Sign in to reply
  • Cancel

Top Replies

  • Gough Lui
    Gough Lui over 2 years ago +6
    94V-0 is a flammability standard. You'll see it all over various PCBs - nothing to do with voltage. Strobing could be due to a bad bootstrap capacitor or main DC storage capacitor that has lost too much…
  • robogary
    robogary over 2 years ago +6
    It was the chopper electrolytic capacitor that was breaking over to cause the worklight strobing. A small 50v 10 uF, I only had 150v on hand for replacement. The removed capacitor didn't give a consistent…
  • javagoza
    javagoza over 2 years ago in reply to shabaz +4
    I have dismantled all the LED bulbs that were damaged at home and so far all the ones that have started to blink have been due to what Shabaz said, a defective LED, they start blinking, with a little bump…
Parents
  • e14phil
    e14phil over 2 years ago

    I'm going to put on my tin foil hat here a little, when LEDS first hit the market for consumer use, they had an expected lifetime of 5-10 years. But as I drive around the UK with a large portion of the infrastructure being converted to LED, its like I am in a disco!  Strobe-ing really feels like the main failure mode.  I wonder if it is intentionally cutting costs, or even some sort of planned obsolescence that causing this. I look forward to reading about what component failure causes the strobing.  

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 2 years ago in reply to e14phil

    There's a book called "LED: A history of the future of lighting" which is a fascinating read. It does mention some unfriendly things that parts of the lighting industry did from time to time (e.g. two companies had a monopoly on fluorescent tube ballasts, and they didn't want them to be replaced with energy-efficient electronic ballasts).

    Back in the 2000's there was some $1M US government prize for the first firm that could make an LED bulb that would be as good as a 60W tungsten one. I think Philips won that prize. It was technically difficult because of the shape and dimensions of the bulb (getting heat out, because of LED inefficiencies at that time).  Philips used some fancy heatsinking for that.

    The flickering can often happen when there's a faulty LED in the chain, sometimes knocking it makes a difference! : )

    For the last few years, I've not had an LED bulb failure (got perhaps 20 in legacy fixtures, i.e. they are not optimised to be LED lighting, but to replace tungsten), but they definitely dim after a couple of years of heavy use (since it's so dark in the UK for half of the year!). 

    Recently I used "bayonet to E22 Edison" adapters, because then there's more space inside the bulb for the electronics. There seems to be a much better choice of E22 bulbs than bayonet. So now there are super-bright lights in a couple of rooms, perhaps too much! But nice when working.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • javagoza
    javagoza over 2 years ago in reply to shabaz

    I have dismantled all the LED bulbs that were damaged at home and so far all the ones that have started to blink have been due to what Shabaz said, a defective LED, they start blinking, with a little bump they go back to normal but eventually time they melt and you see a black dot in the middle of the LED that was defective. Since they go in series, the whole set goes into the "I'll use it for some project" box.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • javagoza
    javagoza over 2 years ago in reply to javagoza

    One example

    image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 2 years ago in reply to shabaz
    shabaz said:
    I think Philips won that prize.

    Philips also produced the long life 'Dubai lamp'. Big Clive did a video on them a couple of years ago to see what's different about the design

    https://www.youtube.com/watch?v=klaJqofCsu4

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • robogary
    robogary over 2 years ago in reply to javagoza

    Is that bulb 120V or 220V ?   I'm not sure if it makes a difference if the power supply is current limited, except the peak volts are higher.  

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • robogary
    robogary over 2 years ago in reply to javagoza

    Is that bulb 120V or 220V ?   I'm not sure if it makes a difference if the power supply is current limited, except the peak volts are higher.  

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • javagoza
    javagoza over 2 years ago in reply to robogary

    220V