Power & Energy
  • Technologies
  • More
Power & Energy
Forum LED Worklight and teardown
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 26 replies
  • Subscribers 281 subscribers
  • Views 6175 views
  • Users 0 members are here
  • robogary
  • power_supply
  • power_conversion
Related

LED Worklight and teardown

robogary
robogary over 2 years ago

My workshop areas have eight 4 foot double tube fluorescent worklights in the man-cave. I installed the 4 foot floursecent fixtures 35 years ago. 

As the tubes fail,  they get consolidated, and one by one empty fluorescent fixtures get replaced with LED worklights. 5 of 8 fluorescents are still in service.

One of the LED worklights failed after a couple years of service. The failure is weird, the worklight had turned into a strobe light. 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Maybe the light can be repaired ?

I dunno, but the opportunity to troubleshoot, reverse engineer,  and maybe even scavenge parts is too good an opportunity to pass up. 

The endcaps are removed from the light fixture. The simplicity is smart. An extruded aluminum tube body, diffuser slides into it, and an LED strip is mounted on the AL extrusion.

image

The power supply leads were desoldered and the LED strip slide right out.  

The LED strip is on a thin fiberglas pcb with 78 COB LED packages soldered in place.The LED strip is labeled with 94v. 

Its easy to follow the traces to see the LED strip has 3 parallel circuits of 26 COB LEDS in series. 

image

Since the LED fixture was strobing, the LEDs seem OK, but the power supply would collapse after being able to start. 

The power supply was tucked inside the aluminum extrusion, encased in an insulated tube.

image

The power supply was first inspected for failed components. The parts are really packed in there. 

Voila !  Nothing smoked. That black thing looks like its had an overtemp near the body. Its labeled L1, ah...an inductor. 

After desoldering and removing, a closer look seems that the inductor had bitty wire leads soldered onto the stiffer component leads.

Ohm check shows its not dead shorted, and LCR meter sez its 1.86 mH. Darn, that seems reasonable. 

The inductor probably isn't bad so it will have to be reinstalled onto the power supply card.

image

Next step is to do reverse engineering on the power supply card to identify components. 

Its for sure a 120VAC 60 Hz to ~ 80Vdc (?) switching power supply, and appears to have 2 stages.  I'll need to surf for info on switching power supply basics.

 If anyone who has alot of design or service experience on switching power supplies, it would be appreciated to share some insights and hints  :-) 

  • Sign in to reply
  • Cancel

Top Replies

  • Gough Lui
    Gough Lui over 2 years ago +6
    94V-0 is a flammability standard. You'll see it all over various PCBs - nothing to do with voltage. Strobing could be due to a bad bootstrap capacitor or main DC storage capacitor that has lost too much…
  • robogary
    robogary over 2 years ago +6
    It was the chopper electrolytic capacitor that was breaking over to cause the worklight strobing. A small 50v 10 uF, I only had 150v on hand for replacement. The removed capacitor didn't give a consistent…
  • javagoza
    javagoza over 2 years ago in reply to shabaz +4
    I have dismantled all the LED bulbs that were damaged at home and so far all the ones that have started to blink have been due to what Shabaz said, a defective LED, they start blinking, with a little bump…
Parents
  • robogary
    robogary over 2 years ago

    ROFL - most of the way to drawing up the schematic, a tiny 6 lead SMD IC maybe trigger chip cant seem to identify. Got thrown a bit, expecting flyback transformers, the board silkscreen identifies the components as L1 & L2, these chokes have 3 leads , and the 2 inductors are wired in parallel using the 3 leads. Unclear if center tapped, or some other relationship. While in the circuit, its really hard to tell if I'm reading coils or not.  

    There are alot of RTV globs on the components that had to be removed to trace. I did find a poor solder joint in the output in one of the RTV globs, so fixed that, reinstalled a previously removed inductor. 

    Resoldered together and the LED light now works on the bench. Mysteriously cant be sure if its from bending leads and components, or by resoldering. Left the light run for awhile, looking good.

    A few hours later, retry again, finally, starts flashing again. Started spraying components with Keyboard Duster (after shaking the can which it says not to do  )  , the LEDs flickered then came back on full again. I suspect it maybe the output cap. Will have to wait to it to mess up again, then replace it to see what happens.  

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rlewicki
    rlewicki over 2 years ago in reply to robogary

    Again, seems like not the only time it was due to a cap.  Also, the cap isn’t catastrophically defective, no bloating, no leaking, just thermally unstable and seems to short internally at some point.  I have witnessed this in other LED lights that were guaranteed 17 years and yet failed after one year or so.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • rlewicki
    rlewicki over 2 years ago in reply to robogary

    Again, seems like not the only time it was due to a cap.  Also, the cap isn’t catastrophically defective, no bloating, no leaking, just thermally unstable and seems to short internally at some point.  I have witnessed this in other LED lights that were guaranteed 17 years and yet failed after one year or so.