Power & Energy
  • Technologies
  • More
Power & Energy
Forum Troubleshooting a PCB
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 281 subscribers
  • Views 1458 views
  • Users 0 members are here
Related

Troubleshooting a PCB

uxphil
uxphil over 2 years ago

imageHi, hoping to get a little help here with a basic PCB trouble shooting question 

I have a kids toy here, which runs of 3aa batteries 

it’s a roof of a train station that has two buttons and should make a noise when either is pressed 

I get some noise, but not at all the right ones

i took it all apart and found this PCB.

i suspect one of the elements it busted. 

question, how to I check whether the following are working 

- capacitors

- resistors 

- diodes 

I’ve tested the speaker and it works 

any other tips on how to troubleshoot this with an multimeter?

What order should I test in? And which settings?

thanks for any help!

Phil

  • Sign in to reply
  • Cancel

Top Replies

  • beacon_dave
    beacon_dave over 2 years ago +2
    Can you add a picture of the reverse of the circuit board and showing the rest of the connections ? Tracing the connections and making a rough sketch of the circuit as a schematic is usually helpful…
  • beacon_dave
    beacon_dave over 2 years ago in reply to uxphil +2
    Have you measured the voltage at the circuit board (red & black wires) when powered up ? If it is significantly lower than the 4.5V expected, then you may find that the glob top doesn't work properly…
  • shabaz
    shabaz over 2 years ago +2
    Those two cylindrical electrolytic capacitors visible in the photo might have dried up. Probably worth replacing them, since that's a low-cost thing to do. Other than that, I can't think of anything much…
Parents
  • beacon_dave
    0 beacon_dave over 2 years ago

    Can you add a picture of the reverse of the circuit board and showing the rest of the connections ?

    Tracing the connections and making a rough sketch of the circuit as a schematic is usually helpful.

    I'm seeing what looks like a battery box with power switch, a microphone and speaker with simple amplifier but don't see any button or power connections to the circuit board. Are the blue wires the button connections ?

    Does the microphone work ? What sort of sounds are you expecting ? Is there another sound effects module ?

    There is some residue and corrosion visible on the board so looks like something has leaked at some point.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • uxphil
    0 uxphil over 2 years ago in reply to beacon_dave

    Here you go image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 2 years ago in reply to uxphil

    And there it is... a glob top COB chip producing the sound effects.

    If that has failed, then you are likely looking at an upcycling project.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 2 years ago in reply to uxphil

    Have you measured the voltage at the circuit board (red & black wires) when powered up ?

    If it is significantly lower than the 4.5V expected, then you may find that the glob top doesn't work properly affecting your sounds.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • beacon_dave
    0 beacon_dave over 2 years ago in reply to uxphil

    Have you measured the voltage at the circuit board (red & black wires) when powered up ?

    If it is significantly lower than the 4.5V expected, then you may find that the glob top doesn't work properly affecting your sounds.