Power & Energy
  • Technologies
  • More
Power & Energy
Forum Safety of plugin solar?
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 281 subscribers
  • Views 1083 views
  • Users 0 members are here
Related

Safety of plugin solar?

Workshopshed
Workshopshed 10 months ago

Just seen a YouTube short from JerryRigEverything for a 4 panel solar system with roof top microinvertors.

The "interesting" feature is that it connects into a regular socket i.e. the power is provided through a plug.Jerry states this is only approved in Utah at the moment and is limited on the size of the system you can install.

For me this raises a couple of questions, firstly how it doesn't electrocute the person handling the plug? But how it doesn't back power the grid when there is a power outage?

I have a solar system at home and it is hard wired with a number of protective devices and isolators between the solar and mains.

Anyone know anything about these plugin systems?

  • Sign in to reply
  • Cancel

Top Replies

  • obones
    obones 10 months ago +2
    They are quite common in Europe and periodically tests for the presence of power coming into the wall socket to decide if it injects power into it. Basically, if it "sees" 220V on its power line then the…
Parents
  • obones
    obones 10 months ago

    They are quite common in Europe and periodically tests for the presence of power coming into the wall socket to decide if it injects power into it.
    Basically, if it "sees" 220V on its power line then the inverter will send its power, and it repeats that test at rapid frequency so as to stop immediately when "street power" goes out.

    Note that it's the same with the solar panels I have here, that are fitted to the roof with their micro inverters connected to the main power panel. If there is no power coming from the utility provider, they don't generate anything either, so as to protect everyone in the street.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Workshopshed
    Workshopshed 10 months ago in reply to obones

    My solar and battery will go off if I lose mains. There was a disconnect option but that was a other £500 and we don't get a lot of power cuts around here.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • ralphjy
    ralphjy 10 months ago in reply to Workshopshed

    I have an older system with an SMA string inverter that has a disconnect that allows me to use the panels when the grid is down. Unfortunately, it is limited to 1.5 KW.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • ralphjy
    ralphjy 10 months ago in reply to Workshopshed

    I have an older system with an SMA string inverter that has a disconnect that allows me to use the panels when the grid is down. Unfortunately, it is limited to 1.5 KW.