Power & Energy
  • Technologies
  • More
Power & Energy
Forum Replacing watch batteries with a USB rechargable cell
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 282 subscribers
  • Views 860 views
  • Users 0 members are here
  • batteries
Related

Replacing watch batteries with a USB rechargable cell

mrmunnz
mrmunnz over 9 years ago

Hi Guys,

 

I'm very new to working with electronics but figured this was a good place to start!

 

I have a device that is currently powered by 2x Maxwell SR1120W Batteries (http://www.batteriesinaflash.com/maxell-silver-oxide-watch-battery-sr1120w-high-drain-replaces-391).  I want to replace these batteries with some kind of USB rechargeable cell - seeing as I have the specs of the Maxwell units, I wanted to find out if it would be as straight forward as just pulling these out, and wiring in a different kind of cell - I have zero idea how the recharge side of batteries work (would I need additional parts to indicate when the cell was fully charged, etc?).

 

I appreciate how stupid this question must sound but if anyone has any advice or could point me in a good direction to start with, that would be greatly appreciated.

  • Sign in to reply
  • Cancel
Parents
  • dougw
    dougw over 9 years ago

    Presumably the 2 batteries are in series to produce 3.1 Volts.

    A single rechargeable Lithium coin cell like a Panasonic ML1220 will have a nominal voltage of 3 volts.

    It is a bit wider but it might work...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mrmunnz
    mrmunnz over 9 years ago in reply to dougw

    Thanks Douglas - this is exactly the kind of starting point I'm after!  The size of the batteries don't really matter (if i end up with a non-coin style battery that is ok) but this looks great.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • mrmunnz
    mrmunnz over 9 years ago in reply to dougw

    Thanks Douglas - this is exactly the kind of starting point I'm after!  The size of the batteries don't really matter (if i end up with a non-coin style battery that is ok) but this looks great.