Power & Energy
  • Technologies
  • More
Power & Energy
Forum Battery Vs Super Capacitor
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 284 subscribers
  • Views 878 views
  • Users 0 members are here
  • super capacitor
  • battery
  • power
Related

Battery Vs Super Capacitor

yadhu22krish@gmail.com
yadhu22krish@gmail.com over 8 years ago

Hi all,

 

Battery Vs super capacitor. Sounds simple, but the replacement of battery into super capacitor is happening in a full speed in a lot of applications. When I briefly studied them Both have its own pros and cons,(Size,capacity,charging and discharging rate,life cycle etc...).I want to know others opinion also. Is it possible to replace battery with super capacitor in coming years ?

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 8 years ago +2
    Hi, I feel it will be possible to use super capacitors instead of batteries for special applications. Devices that are not size sensitive and run on very low currents may already be good candidates particularly…
  • mikec.vina
    mikec.vina over 8 years ago +2
    Road maps are being developed and yes, over the years, the Super Capacitor will take on more and more roles of Batteries. Keep an eye on the Farnell site for the new Hybrid Lithium Capacitors soon to be…
Parents
  • jw0752
    jw0752 over 8 years ago

    Hi,

    I feel it will be possible to use super capacitors instead of batteries for special applications. Devices that are not size sensitive and run on very low currents may already be good candidates particularly for situations where routine charging is available. This is made possible by switch mode power supplies which can take a varying voltage input and provide a stable output voltage to power a device.

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • jlangbridge
    jlangbridge over 8 years ago in reply to jw0752

    I think that there are some Silicon Labs STK evaluation kits that use super capacitors for RTC timekeeping and RAM retention in deep sleep. They are "small", since only used for RTC timekeeping, but do have the advantage of recharging in a split second when connected to the PC.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • jlangbridge
    jlangbridge over 8 years ago in reply to jw0752

    I think that there are some Silicon Labs STK evaluation kits that use super capacitors for RTC timekeeping and RAM retention in deep sleep. They are "small", since only used for RTC timekeeping, but do have the advantage of recharging in a split second when connected to the PC.