Power & Energy
  • Technologies
  • More
Power & Energy
Forum Solar panels in gasoline car
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 11 replies
  • Subscribers 285 subscribers
  • Views 6320 views
  • Users 0 members are here
Related

Solar panels in gasoline car

pmfman
pmfman over 7 years ago

We all know that an alternator in a car uses a significant portion of a car's HP, thus lots of its fuel efficiency. Thus in theory, if a large enough solar panel (lets say 150 watts) wouldn't this decrease the load on the alternator this increasing HP/fuel efficiency?

 

This is more or less to satisfy curiosity, I don't intend to try it.

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 7 years ago +7
    Solar panels could help reduce fuel consumption and it is even possible to run vehicles solely on solar power. It is mainly a question of how much to spend versus how much is the benefit, including factors…
  • 14rhb
    14rhb over 7 years ago +6
    Hi Peter, A very good suggestion which has got me thinking early on a Sunday morning. I don't know what a typical alternator loads an engine by but it goes from a large amount (that you wish to reduce…
  • Pavel.Simon
    Pavel.Simon over 7 years ago +4
    Interesting idea, but. One things is produce additional electricity with solar panels, whatever during drive or during car waiting somewhere. But for reducing looses on alternator, you would need think…
Parents
  • kkazem
    kkazem over 6 years ago

    The efficiency gain would be highly dependent on the size of the car, car's engine, and alternator load. For a large V6 or V8 vehicle, the alternator can easily have a 100 amp capacity, or nominally 1200 watts (12V * 100A). In that case, a 150W solar panel would do little to affect engine efficiency. But typically, the alternator is running a load of only a small fraction of its capacity. So the solar panels would only even help much if the electrical system load was high.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • kkazem
    kkazem over 6 years ago

    The efficiency gain would be highly dependent on the size of the car, car's engine, and alternator load. For a large V6 or V8 vehicle, the alternator can easily have a 100 amp capacity, or nominally 1200 watts (12V * 100A). In that case, a 150W solar panel would do little to affect engine efficiency. But typically, the alternator is running a load of only a small fraction of its capacity. So the solar panels would only even help much if the electrical system load was high.