Power & Energy
  • Technologies
  • More
Power & Energy
Forum Solar panels in gasoline car
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 11 replies
  • Subscribers 285 subscribers
  • Views 6344 views
  • Users 0 members are here
Related

Solar panels in gasoline car

pmfman
pmfman over 7 years ago

We all know that an alternator in a car uses a significant portion of a car's HP, thus lots of its fuel efficiency. Thus in theory, if a large enough solar panel (lets say 150 watts) wouldn't this decrease the load on the alternator this increasing HP/fuel efficiency?

 

This is more or less to satisfy curiosity, I don't intend to try it.

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 7 years ago +7
    Solar panels could help reduce fuel consumption and it is even possible to run vehicles solely on solar power. It is mainly a question of how much to spend versus how much is the benefit, including factors…
  • 14rhb
    14rhb over 7 years ago +6
    Hi Peter, A very good suggestion which has got me thinking early on a Sunday morning. I don't know what a typical alternator loads an engine by but it goes from a large amount (that you wish to reduce…
  • Pavel.Simon
    Pavel.Simon over 7 years ago +4
    Interesting idea, but. One things is produce additional electricity with solar panels, whatever during drive or during car waiting somewhere. But for reducing looses on alternator, you would need think…
Parents
  • pmfman
    pmfman over 7 years ago

    So essentially it isnt practical on a car unless the size of solar panels reduces or unless the entire horizontal surface of the car is solar panels

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Pavel.Simon
    Pavel.Simon over 7 years ago in reply to pmfman

    Standard Poly/Mono crystalline PV panels costs about 0,5 €/Wp. From 1 m2 you can get about 140 - 160 Wp. But those framed PV panels are not good choice.

    Better is use flexible panels, but they cost about 1,5 to 2 €/Wp. Efficiency is similar -  140 to 160 Wp/m2. You could easily up to 2 m2 on car roof - about 300 Wp on roof. This give you somewhere about 450 to 600 € per roof with flexible PV panel.

    But than you need another components (cables, charger, some control and safe devices, ...), and easily you are in 1 000 € price level. This give you about 700 l of petrol - and this is (with 7 l/100 km) about 10 000 km of full consumption.

    But with saved consumption on alternator (let say up to 10 %) is 100 000 km return of investment. And this is not covering any necessities of alternator disconnection improvement.

    Result - only with saved fuel make no sense to do it. But with other attributes to consider - learning something new, saving environment, curiosity, ... it is interesting experiment.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Pavel.Simon
    Pavel.Simon over 7 years ago in reply to pmfman

    Standard Poly/Mono crystalline PV panels costs about 0,5 €/Wp. From 1 m2 you can get about 140 - 160 Wp. But those framed PV panels are not good choice.

    Better is use flexible panels, but they cost about 1,5 to 2 €/Wp. Efficiency is similar -  140 to 160 Wp/m2. You could easily up to 2 m2 on car roof - about 300 Wp on roof. This give you somewhere about 450 to 600 € per roof with flexible PV panel.

    But than you need another components (cables, charger, some control and safe devices, ...), and easily you are in 1 000 € price level. This give you about 700 l of petrol - and this is (with 7 l/100 km) about 10 000 km of full consumption.

    But with saved consumption on alternator (let say up to 10 %) is 100 000 km return of investment. And this is not covering any necessities of alternator disconnection improvement.

    Result - only with saved fuel make no sense to do it. But with other attributes to consider - learning something new, saving environment, curiosity, ... it is interesting experiment.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Children
  • enertechupsindia
    enertechupsindia over 6 years ago in reply to Pavel.Simon

    Very good point and thanks for valuable info.