Power & Energy
  • Technologies
  • More
Power & Energy
Forum Solar panels in gasoline car
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 11 replies
  • Subscribers 285 subscribers
  • Views 6338 views
  • Users 0 members are here
Related

Solar panels in gasoline car

pmfman
pmfman over 7 years ago

We all know that an alternator in a car uses a significant portion of a car's HP, thus lots of its fuel efficiency. Thus in theory, if a large enough solar panel (lets say 150 watts) wouldn't this decrease the load on the alternator this increasing HP/fuel efficiency?

 

This is more or less to satisfy curiosity, I don't intend to try it.

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 7 years ago +7
    Solar panels could help reduce fuel consumption and it is even possible to run vehicles solely on solar power. It is mainly a question of how much to spend versus how much is the benefit, including factors…
  • 14rhb
    14rhb over 7 years ago +6
    Hi Peter, A very good suggestion which has got me thinking early on a Sunday morning. I don't know what a typical alternator loads an engine by but it goes from a large amount (that you wish to reduce…
  • Pavel.Simon
    Pavel.Simon over 7 years ago +4
    Interesting idea, but. One things is produce additional electricity with solar panels, whatever during drive or during car waiting somewhere. But for reducing looses on alternator, you would need think…
  • kkazem
    kkazem over 6 years ago

    The efficiency gain would be highly dependent on the size of the car, car's engine, and alternator load. For a large V6 or V8 vehicle, the alternator can easily have a 100 amp capacity, or nominally 1200 watts (12V * 100A). In that case, a 150W solar panel would do little to affect engine efficiency. But typically, the alternator is running a load of only a small fraction of its capacity. So the solar panels would only even help much if the electrical system load was high.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<