Power & Energy
  • Technologies
  • More
Power & Energy
Forum Question about using ATX PSU for DC Power
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 15 replies
  • Subscribers 284 subscribers
  • Views 2226 views
  • Users 0 members are here
Related

Question about using ATX PSU for DC Power

tech3475
tech3475 over 7 years ago

Hi, my apologies if this is the wrong place to ask but it seemed like it made the most sense.

 

In a few months I'm going to be putting my Amiga 1200 into a new case and power it using an ATX PSU, one thing I'd also like to do as part of this project is to internalize the scan doubler I use at the same time and power it using the ATX PSU.

 

The Scan Doubler in question is a GBS-8220, according to the manual (link: https://www.mikesarcade.com/estore/datasheets/GBS-8200-booklet.pdf), it can take 5V 2A but the issue I have is how to power it safely.

 

The original idea was just to solder it to a molex connector on the 5V rail and power it directly, but I'm concerned over whether this is safe without some kind of protection in place (I've seen resistors used for example or a fuse for similar purposes).

 

The other idea is to get some kind of circuit regulator and possibly use the 12V rail, stepping down to 5V.

 

Any advice is appreciated.

 

Thank you.

  • Sign in to reply
  • Cancel

Top Replies

  • rusgray
    rusgray over 7 years ago +3
    Looking at the board photo on the data sheet you linked to, it sure seems like there's an inline PTC fuse on the board right before what looks to me like an input reservoir cap. I assume both the barrel…
  • rusgray
    rusgray over 7 years ago in reply to 14rhb +2
    You're correct; the part that I thought might be a fuse has the reference designator 'D2' in that clearer photo, making it a diode.
  • tech3475
    tech3475 over 7 years ago +2
    I should give more details. The Amiga mobo is going to be put in a new case and powered by the PSU using the standard motherboard connector via an adapter I’m buying. The Scan Doubler I plan on powering…
Parents
  • tech3475
    tech3475 over 7 years ago

    I should give more details.

     

    The Amiga mobo is going to be put in a new case and powered by the PSU using the standard motherboard connector via an adapter I’m buying.

     

    The Scan Doubler I plan on powering through the molex connector you’d typically use for disk drives using a spare molex plug I have. So in the case of say that adapter I mentioned earlier, it would be used only for the Scan Doubler and nothing else.

     

    I already have an external DC adapter for the scan doubler but I’m trying to internalise it if possible.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • 14rhb
    14rhb over 7 years ago in reply to tech3475

    powered by the PSU

    Is this the ATX PSU you are looking at using?

     

    I think some pictures of what you have would help the E14 community to make better suggestions.

     

    ps: glad to see the Amiga is still being used. In my opinion the Amiga and Atari 1040ST were great computers that brought low-cost processing up to another level; appealing to both professional and gaming users.

     

    Rod

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • tech3475
    tech3475 over 7 years ago in reply to 14rhb

    As of now I still haven't purchased the actual PSU I'm going to use.

     

    To provide context, this is what I'm getting for my Amiga 1200:

    Case: https://www.checkmate1500plus.com/Products.aspx?id=342

     

    The Power for the Amiga's motherboard is being provided by this:

    https://www.checkmate1500plus.com/Products.aspx?id=357

     

    In terms of the actual PSU, it has to be in the SFX format factor (basically a smaller ATX PSU). I've yet to decide on which one to buy, although this one has been bought up:

    https://www.amazon.co.uk/gp/product/B06X6HFR2K/

     

    I have a spare (female) 3.5" molex connector lying around from a fan similar to this:

    https://image.made-in-china.com/43f34j00YjOTKVSyLEke/8cm-PC-Case-Cooler-Fan-4-Pin-Molex-KCF-1000-.jpg

     

    With which I'm going to use to connect to the Scan Doubler in some way using the supplied cable by soldering where necessary (see the lower right of this image for the cable):

    https://images.yaoota.com/SVYk42TFlf2nEzUi_TrRqz_nbHE=/trim/yaootaweb-production-ng/media/crawledproductimages/7dffa0747…

     

    I never liked having the Scan Doubler being exposed on the side of my 1200, so one of my goals is to put the Scan Doubler inside the above case (obviously isolating it from the case) and powering it from the PSU as I'm hoping this will become a better setup (e.g. not needing a second external adapter and powering it on when I power on the Amiga).

     

    I hope this helps.

     

    BTW, the Amiga community is still quite surprisingly active, if niche, just recently they released Workbench 3.1.4 which I also plan on installing.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • tech3475
    tech3475 over 7 years ago in reply to 14rhb

    As of now I still haven't purchased the actual PSU I'm going to use.

     

    To provide context, this is what I'm getting for my Amiga 1200:

    Case: https://www.checkmate1500plus.com/Products.aspx?id=342

     

    The Power for the Amiga's motherboard is being provided by this:

    https://www.checkmate1500plus.com/Products.aspx?id=357

     

    In terms of the actual PSU, it has to be in the SFX format factor (basically a smaller ATX PSU). I've yet to decide on which one to buy, although this one has been bought up:

    https://www.amazon.co.uk/gp/product/B06X6HFR2K/

     

    I have a spare (female) 3.5" molex connector lying around from a fan similar to this:

    https://image.made-in-china.com/43f34j00YjOTKVSyLEke/8cm-PC-Case-Cooler-Fan-4-Pin-Molex-KCF-1000-.jpg

     

    With which I'm going to use to connect to the Scan Doubler in some way using the supplied cable by soldering where necessary (see the lower right of this image for the cable):

    https://images.yaoota.com/SVYk42TFlf2nEzUi_TrRqz_nbHE=/trim/yaootaweb-production-ng/media/crawledproductimages/7dffa0747…

     

    I never liked having the Scan Doubler being exposed on the side of my 1200, so one of my goals is to put the Scan Doubler inside the above case (obviously isolating it from the case) and powering it from the PSU as I'm hoping this will become a better setup (e.g. not needing a second external adapter and powering it on when I power on the Amiga).

     

    I hope this helps.

     

    BTW, the Amiga community is still quite surprisingly active, if niche, just recently they released Workbench 3.1.4 which I also plan on installing.