Power & Energy
  • Technologies
  • More
Power & Energy
Forum Question about using ATX PSU for DC Power
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 15 replies
  • Subscribers 284 subscribers
  • Views 2221 views
  • Users 0 members are here
Related

Question about using ATX PSU for DC Power

tech3475
tech3475 over 7 years ago

Hi, my apologies if this is the wrong place to ask but it seemed like it made the most sense.

 

In a few months I'm going to be putting my Amiga 1200 into a new case and power it using an ATX PSU, one thing I'd also like to do as part of this project is to internalize the scan doubler I use at the same time and power it using the ATX PSU.

 

The Scan Doubler in question is a GBS-8220, according to the manual (link: https://www.mikesarcade.com/estore/datasheets/GBS-8200-booklet.pdf), it can take 5V 2A but the issue I have is how to power it safely.

 

The original idea was just to solder it to a molex connector on the 5V rail and power it directly, but I'm concerned over whether this is safe without some kind of protection in place (I've seen resistors used for example or a fuse for similar purposes).

 

The other idea is to get some kind of circuit regulator and possibly use the 12V rail, stepping down to 5V.

 

Any advice is appreciated.

 

Thank you.

  • Sign in to reply
  • Cancel

Top Replies

  • rusgray
    rusgray over 7 years ago +3
    Looking at the board photo on the data sheet you linked to, it sure seems like there's an inline PTC fuse on the board right before what looks to me like an input reservoir cap. I assume both the barrel…
  • rusgray
    rusgray over 7 years ago in reply to 14rhb +2
    You're correct; the part that I thought might be a fuse has the reference designator 'D2' in that clearer photo, making it a diode.
  • tech3475
    tech3475 over 7 years ago +2
    I should give more details. The Amiga mobo is going to be put in a new case and powered by the PSU using the standard motherboard connector via an adapter I’m buying. The Scan Doubler I plan on powering…
Parents
  • tech3475
    tech3475 over 7 years ago

    Does anyone have any experience/opinions of converters such as this for my type of usage:

    https://www.amazon.co.uk/Lorjoy-CPT-UL-1-Converter-Regulator-Vehicular/dp/B07FXR6TNF

     

    Bearing in mind the information I posted before (i.e. this will only power the Scan Doubler and nothing else), is something like this ok?

     

    I would test any such device before installation.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • tech3475
    tech3475 over 7 years ago

    Does anyone have any experience/opinions of converters such as this for my type of usage:

    https://www.amazon.co.uk/Lorjoy-CPT-UL-1-Converter-Regulator-Vehicular/dp/B07FXR6TNF

     

    Bearing in mind the information I posted before (i.e. this will only power the Scan Doubler and nothing else), is something like this ok?

     

    I would test any such device before installation.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • michaelkellett
    michaelkellett over 7 years ago in reply to tech3475

    A decent industrial quality 15W DC-DC converter will cost about £28 (cheapest 5V 3A Traco converter stocked by Farnell).

     

    if you pay £2.06 for one it may work, it may even work quite well. I wouldn't connect it to anything I cared about not blowing up.

     

    There is no way of telling how reliable it will be and how it may fail. It might also be noisy (electrically) and almost certainly won't comply with EMC standards.

     

    If you test it, run it at the working load for at least 48 hours and it still looks OK then you may well get away with it.

     

    How much is the scan doubler worth ?

     

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • tech3475
    tech3475 over 7 years ago in reply to michaelkellett

    Around £20, but the risk of high EM is off putting so thanks for the info.