Power & Energy
  • Technologies
  • More
Power & Energy
Forum Automatic generator start
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 284 subscribers
  • Views 1515 views
  • Users 0 members are here
Related

Automatic generator start

andrequeiroz.com
andrequeiroz.com over 7 years ago

My electricity grid is dropping frequently. When the power drops, I have to manually connect a small diesel generator.

I would like to use a raspberry to automate the triggering of the generator.

Which sensor should I use to detect the power drop ?

 

ops: 380v

 

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 7 years ago +3
    It would seem that you need a battery or uninterruptible power supply to run the Raspberry Pi when the power fails. A simpler method would be to have a relay that is powered by mains voltage. When the…
  • jw0752
    jw0752 over 7 years ago +3
    Hi Andre, I like dougw suggestion and I would also look to include some sort of Hysteresis so that once the relay triggers the start of the generator and the switching of the power grid from external to…
  • a531016
    a531016 over 7 years ago +3
    Andre, The simplist verson of monitoring mains voltage is a relay with a 380V coil, and a normally closed secondary. This would open on power failure, and the RPI can start the generator (assuming an electronic…
Parents
  • a531016
    a531016 over 7 years ago

    Andre,

     

    The simplist verson of monitoring mains voltage is a relay with a 380V coil, and a normally closed secondary. This would open on power failure, and the RPI can start the generator (assuming an electronic ignition).

     

    Please remember to introduce a delay on start up and shut down - out of phase generator and mains electricity on grid restoration will blow everything up! This could be a 2 pole relay (phase and neutral) with a timed delay switching from mains to generator. This is where the UPS would come in.

     

    In commercial installations, the critical load is driven by a UPS, with perhaps 20 minutes of autonomy. The UPS input would have 2 feeds, mains and a generator backup. In normal operation the mains charges the UPS and powers the Critical devices. When power fails, critical devices are supplied by the batteries, the supply changes over and the generator starts to charge the batteries. Some other supplies may be deemed necessary, which will be generator supplied, but 15 -20 seconds of generator start up is acceptable. On restoration of power the generator will shut down and mains power will switch over.

     

    ATS (automatic transfer switches) are the commercial switching product, but a good quality relay / contactor with a delay would do.

     

    Of course, if you are having brown outs, not just blackouts, that's a whole different thing. Then you are definitely into phase monitoring (I would reccomend a meter with Modbus, some have aux output contacts that can drive relays).

     

    I hope that makes sense and helps!

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • a531016
    a531016 over 7 years ago

    Andre,

     

    The simplist verson of monitoring mains voltage is a relay with a 380V coil, and a normally closed secondary. This would open on power failure, and the RPI can start the generator (assuming an electronic ignition).

     

    Please remember to introduce a delay on start up and shut down - out of phase generator and mains electricity on grid restoration will blow everything up! This could be a 2 pole relay (phase and neutral) with a timed delay switching from mains to generator. This is where the UPS would come in.

     

    In commercial installations, the critical load is driven by a UPS, with perhaps 20 minutes of autonomy. The UPS input would have 2 feeds, mains and a generator backup. In normal operation the mains charges the UPS and powers the Critical devices. When power fails, critical devices are supplied by the batteries, the supply changes over and the generator starts to charge the batteries. Some other supplies may be deemed necessary, which will be generator supplied, but 15 -20 seconds of generator start up is acceptable. On restoration of power the generator will shut down and mains power will switch over.

     

    ATS (automatic transfer switches) are the commercial switching product, but a good quality relay / contactor with a delay would do.

     

    Of course, if you are having brown outs, not just blackouts, that's a whole different thing. Then you are definitely into phase monitoring (I would reccomend a meter with Modbus, some have aux output contacts that can drive relays).

     

    I hope that makes sense and helps!

    • Cancel
    • Vote Up +3 Vote Down