Power & Energy
  • Technologies
  • More
Power & Energy
Polls Has the time come for the decentralized power grid?
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: rscasny
  • Date Created: 25 Aug 2019 11:08 PM Date Created
  • Last Updated Last Updated: 11 Oct 2021 2:59 PM
  • Views 3198 views
  • Likes 1 like
  • Comments 18 comments
Related
Recommended

Has the time come for the decentralized power grid?

In some circles, the centralized power grid most nations have is on par with the dinosaur: big, clumsy and a thing of the past.

 

Whether it be the excessive costs of building and maintaining a centralized power grid, the occurrence of too many power blackouts from centralized power, or the risk of hackers and other bad actors impacting its power reliability, the need for a decentralized power grid on a national scale is critical to human civilization.

 

A decentralized power grid can include solar, geothermal, wind, or any number of innovative renewable technologies. They can include microgrids or even what I like to call the home grid. Power is generated locally and more cost effectively.

 

Here's the question: Has the time come for the decentralized power grid?

  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • dougw
    dougw over 7 years ago +6
    The time has come for central power grids to be augmented (not replaced) by small local power sources. When this becomes a significant portion of the total power and we start to depend on it, I expect…
  • DAB
    DAB over 7 years ago +5
    My local power net has been so unreliable that I installed a whole house generator about 5 years ago. Now while my neighbors are in the dark, I have full power. So I would have to encourage everyone to…
  • ntewinkel
    ntewinkel over 7 years ago in reply to clem57 +4
    True, and in some cases power is more easily generated in one community than another, so moving power around works well. I would like to see it more decentralized in the form of having each community,…
Parents
  • DAB
    DAB over 7 years ago

    My local power net has been so unreliable that I installed a whole house generator about 5 years ago.

    Now while my neighbors are in the dark, I have full power.

     

    So I would have to encourage everyone to set up your own local power source just in case.

    It reduces your dependence and provides you with options should anything happen to your local power network.

     

    DAB

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • 14rhb
    14rhb over 7 years ago in reply to DAB

    Hi DAB , nice to have that assurance, especially during winter months. Do you use a diesel generator?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • 14rhb
    14rhb over 7 years ago in reply to DAB

    Hi DAB , nice to have that assurance, especially during winter months. Do you use a diesel generator?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • DAB
    DAB over 7 years ago in reply to 14rhb

    I use a natural gas generator.

    I tied into my furnace gas feed, so as long as the gas flows I have a generator available.

     

    Last year we had several ice storms in the area, which took down the net during some cold spells.

    We were nice and warm as the furnace still worked, we had running water from the well, and all of our electronics worked so I could do work on my books.

     

    Life is easier when you do not have to worry about losing power.

     

    DAB

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • 14rhb
    14rhb over 7 years ago in reply to DAB

    Sounds like an ideal setup. I always thought such generators also needed electrical power to operate - I know my household gas water boiler does. However it also has its own electrical breaker so I could in theory have a low current backup source (eg solar - batteries - inverter) to get it working. Such a scheme would also be useful to feed into the low power lighting circuits, especially with the advent of high efficiency LED lights.

    [For anyone wanting to do such an approach...check your countries electrical regulations and get a qualified person to modify/inspect/certify if necessary ! ]

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 7 years ago in reply to 14rhb

    The generator came with an automated panel, which switched from the outside grid to the generator after the generator came up to speed and the power stabilized.

    It then throws a big relay that switches most of the house circuits over to the generator.

     

    Once the main power is restored, the relay switches back and the generator shuts off.

     

    Really cool to see. When the lights go out I only have to wait about 30 seconds and the power is back on.

     

    DAB

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • 14rhb
    14rhb over 7 years ago in reply to DAB

    Sounds awesome. If I had that setup I'd actually look forward to a power cut just to try it out !