Power & Energy
  • Technologies
  • More
Power & Energy
Polls Microinverters vs Inverters
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: ojed81
  • Date Created: 25 May 2020 6:25 PM Date Created
  • Last Updated Last Updated: 11 Oct 2021 2:59 PM
  • Views 1834 views
  • Likes 3 likes
  • Comments 8 comments
Related
Recommended

Microinverters vs Inverters

What is the best choice?

  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • genebren
    genebren over 6 years ago +4
    This is really a question of scale. The microinverters are very attractive for smaller arrays, where as the full size inverters can be more cost effective and efficient in larger installations.
  • ralphjy
    ralphjy over 6 years ago +4
    The choice between inverter types is really dependent on the installation constraints and requirements. When I installed my array 2 1/2 years ago I went with a string inverter even though I do get shadowing…
Parents
  • rosylinda
    rosylinda over 6 years ago

    I like to prefer Inverter in comparison to microinverter.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • kkazem
    kkazem over 6 years ago in reply to rosylinda

    As an expert that designs power inverters, i'd say that single inverter vs a distributed inverter network choice depends highly on the application. For most homes, a single inverter is fine. For a large industrial system, a micro-inverter network might be better for reliability and maintenance reasons. There's also a system that uses distributed dc-dc converters on each string of solar panels and the dc from the many converters is combined in series, parallel, or series-parallel and input to a single inverter. This is a very good choice for solar due to high reliability.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • kkazem
    kkazem over 6 years ago in reply to rosylinda

    As an expert that designs power inverters, i'd say that single inverter vs a distributed inverter network choice depends highly on the application. For most homes, a single inverter is fine. For a large industrial system, a micro-inverter network might be better for reliability and maintenance reasons. There's also a system that uses distributed dc-dc converters on each string of solar panels and the dc from the many converters is combined in series, parallel, or series-parallel and input to a single inverter. This is a very good choice for solar due to high reliability.