Robotics
  • Technologies
  • More
Robotics
Blog Baxter industrial robot is not only adaptable but friendly to humans
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Robotics to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 20 Sep 2012 5:48 PM Date Created
  • Views 879 views
  • Likes 0 likes
  • Comments 1 comment
  • research
  • industrial
  • industry
  • manufacturing
  • robotics
  • robot
  • embedded
  • cabeatwell
  • prototyping
  • automation
  • innovation
Related
Recommended

Baxter industrial robot is not only adaptable but friendly to humans

Catwell
Catwell
20 Sep 2012

image

Baxter (via Rethink Robotics)

 

Rethink Robotics has recently unveiled their contribution to the world of robotics and its name is Baxter. The Boston-based company states that the manufacturing robot is not only adaptable to its industrial environment but also safe working side-by-side with its human counterparts (meaning it won’t ‘crush, kill, and destroy’). Baxter was designed for the manufacturing field and purposly equipped with two ambidextrous arms with 7-DOF which feature 2 ‘end-effectors’ that can be outfitted with different attachments such as vacuum cups or electric parallel grippers with interchangeable fingers (depending on the task). Each arm is equipped with force-feedback sensors that immobilize the arm if Baxter inadvertently hits an object such as a human even though the force generated by the robot is negligible on impact (it won’t hurt you).

 

Baxter’s head features 5 independent cameras that it uses to detect objects parts and work-space along with a 3600 sonar detection module. It uses the sensors for detecting humans and obstacles in the immediate work area. The robot uses a screen for its face that provides interaction (or interface) with its human co-workers such as giving it commands or tasks which the robot nods it head if it understands or displays a ‘puzzled’ look if it didn’t quite understand. The robot can also be programmed through direct arm movements through control panels on both of the bots arms (training through demonstration) or through a GUI interface. Baxter can be positioned practically anywhere as it sits on a mobile platform with castors. However, the company states that future revisions of the robot will feature the ability to be ‘self-guided’ on a robotic platform.

 

Repetitive menial labor is what Baxter was designed for and has the ability to handle materials (up to 5 pounds in weight), packing/unpacking, object inspection, light assembly of products and finishing operations (grinding and polishing materials). The robot costs $22,000 US, so most of us won’t have one for our homes. It's relatively cheap enough for small manufacturing companies which is what Rethink Robotics is the intended target.

 

Personally, I don't care for the robot's digital face. It makes me think it's trying to hide something.

 

 

Cabe

http://twitter.com/Cabe_e14

  • Sign in to reply
  • e14 Contributor
    e14 Contributor over 14 years ago

    I have seen the robot at the MIT Technology Review Conference (Emtech2012) in Boston. Roadney Brooks the founder of Rethink Robotics gave a speech: http://livestre.am/4bUQh (at min 18ff). Looking back how Roomba developed this can get very interesting.