Robotics
  • Technologies
  • More
Robotics
Blog HOVIS robot controlled via Android phones
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Robotics to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 17 Jan 2012 9:19 PM Date Created
  • Views 836 views
  • Likes 1 like
  • Comments 3 comments
  • research
  • autonomous
  • hmi
  • robotics
  • robots
  • robot
  • hovis
  • behavior
  • cabeatwell
  • korea
  • automation
  • sensor
  • innovation
Related
Recommended

HOVIS robot controlled via Android phones

Catwell
Catwell
17 Jan 2012

imageimage

(Right) HOVIS bot. (Via Robotshop)  (Left) A less advance HOVIS.

 

Beware Android’s apps are COMING ALIVE!

 

A South Korean company, Dasarobot, invented a HOVIS humanoid robot. The HOVIS can only be compatibility with any 3.5-inch Android-based smartphone. When the phone is connected to HOVIS, the app then become the robot’s commander. Several Android control apps are planned for the HOVIS bot, though availability outside Korea is not clear. However, when searching through your Android app market, I recommend avoiding the violent ones, unless you want a vicious robot.

 

The HOVIS humanoid robot added some new kicks. The leading telecommunications company in South Korea, SK Telecom, has made it possible for the robot to use Wi-Fi and Bluetooth for control. It not only can retrieve data through thin air, but it can also see, hear and even speak. In order for it to become an eye seeking robot, a camera (computer vision), microphone and speaker (speech recognition, speech synthesis), and the processing power of a fixed PC were added to it.

 

Wondering how much it would cost for developing a humanoid robot hobby? The phrase, bang for your buck, holds truth with these robots. You have your choice from inexpensive robots to expensive academic humanoids. The price tag attached to these remarkable robots start only at $620 for the basic. The HOVIS brand gives you many styles to pick from. When choosing the style all of them have complete-with-exoskeleton to DIY kits, and one of four levels of software for beginners to knowledgeable programmers.

 

Cabe
http://twitter.com/Cabe_e14

  • Sign in to reply
Parents
  • fustini
    fustini over 14 years ago

    Do you know if the interface to Android is USB?  I'm wondering if it uses the ADK APIs.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Catwell
    Catwell over 14 years ago in reply to fustini

    It would seem silly not to have USB as an option. However, I can not find USB on the list. It is connected through WiFi and Bluetooth.

     

    You are probably thinking of Google's Arduino-Based ADK from Google I/O 2011?

     

    Cabe

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fustini
    fustini over 14 years ago in reply to Catwell

    Ah ok.  I was curious if it used the USB-based ADK interface like the one robot showed off at I/O that used the Arduino-based ADK reference board.  Wireless is good too as long as the bay for the phone in the robot provides USB power rails at least.

     

    BTW, unrelated but just popped into my head, have you seen RobotGrrl's NFC hats?  http://robotgrrl.com/blog/2011/11/21/robobrrd-and-the-nfc-hats/

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • fustini
    fustini over 14 years ago in reply to Catwell

    Ah ok.  I was curious if it used the USB-based ADK interface like the one robot showed off at I/O that used the Arduino-based ADK reference board.  Wireless is good too as long as the bay for the phone in the robot provides USB power rails at least.

     

    BTW, unrelated but just popped into my head, have you seen RobotGrrl's NFC hats?  http://robotgrrl.com/blog/2011/11/21/robobrrd-and-the-nfc-hats/