Robotics
  • Technologies
  • More
Robotics
Blog Repairing a Vendo V-80 cola dispencer of the 1950s
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Robotics to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 16 Nov 2014 12:31 AM Date Created
  • Views 5809 views
  • Likes 4 likes
  • Comments 13 comments
  • hack
  • vintage
  • repair
Related
Recommended

Repairing a Vendo V-80 cola dispencer of the 1950s

Jan Cumps
Jan Cumps
16 Nov 2014

One of my friends has bought a soft drink bottle cooler as a present for his partner.

The outside of the machine is agreeable, but the state of the electr(on)ics is bad. More than 20 wires have been cut off by previous owners and restorers. The only part that still works is the refrigerator.

image

At this moment I'm assessing the damage done by previous repairs, and building a plan to make the cooler dispense bottles in some way.

 

My current assessment:

- the motor that activates the vending cycle is toast. So is the gear box of that motor.

- the coin validation mechanism is incomplete and doesn't work anymore.

- everywhere I look wires are cut and bodged together in a seemingly random way. Someone had a go at it, but I think that person was not restricted by any relevant knowledge image

 

I'm planning to decipher the circuit (I purchased a service manual on-line), get the basic mechanism working again, and replace the coin detector by  an optical interrupter.


I'm on a deadline. The cooler is for the girlfriend's birthday. And I'm invited late to the party. My design decisions will be guided by time and 'having the parts available at home' more than efficient solutions.

  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 11 years ago +3
    Epilogue: The girl left. Expensive gifts don't guarantee good relations.
  • gadget.iom
    gadget.iom over 11 years ago in reply to Jan Cumps +2
    Well thats a testament to good workmanship!
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to doctorcdf +1
    The Internet of Cola , publish temp, use, stock qty etc on line for all to see, maybe even a WEB cam to post who is at the machine
Parents
  • Jan Cumps
    Jan Cumps over 11 years ago

    Yeah, there is a whole series of mods that can be hacked into the machine. First I could replace the mechanical switches with sensors (optical or magnetic), the cooling thermostat and motor controls are other candidates for modification.

    I can't use the current actuators for low voltage though. The state of the contacts and the amount of bounce is dazzling. It works to activate the 110 V relais, but no chance to get a decent 3.3 or 5V signal.

     

    Some action photos:

    measuring the motor circuit:

    image

     

    coin detector

     

    image

     

    detector proto

     

    image

     

     

    Some hardware:

     

       imageimage

     

    imageimageimage

     

    my proto code

     

    /*
    // vento V-80 controls
    // no copyright jc 2014
     */
    
    // the actuator relais that will engage when coin is detected
    #define RELAIS 8 
    // the analog input signal from IR detection circuit
    #define IR 0
    // how long is the relais actuated when coin detected
    #define PULSE_WIDTH 750
    // at this level (from 0 to 1023) we consider the IR channel interrupted
    #define THREASHOLD 450
    // status led
    #define RELAIS_STATUS_LED 12
    #define IR_STATUS_LED 10
    
    
    
    
    // the setup function runs once when you press reset or power the board
    void setup() {
      // initialize the relais pin, so thzt it always assumes not-engaged status at startup and reset
      pinMode(RELAIS, OUTPUT);
      digitalWrite(RELAIS, LOW);
      // mark the infrared detection pin as input input
      pinMode(IR, INPUT);
      // mark the status led as output
      pinMode(RELAIS_STATUS_LED, OUTPUT);
      digitalWrite(RELAIS_STATUS_LED, LOW);
      pinMode(IR_STATUS_LED, OUTPUT);
      digitalWrite(IR_STATUS_LED, LOW);
      
      
      // debug settings
      Serial.begin(9600);
    }
    
    
    // the loop function runs over and over again forever
    void loop() {
      
      // when a coin is detected, we actuate the relais for the time defined by THREASHOLD
      if (detectCoin()) {
        digitalWrite(RELAIS, HIGH);
        digitalWrite(IR_STATUS_LED, HIGH);
        digitalWrite(RELAIS_STATUS_LED, HIGH);
        delay(50); // pulse the coin detect led for a moment
        digitalWrite(IR_STATUS_LED, LOW);
        
        delay(PULSE_WIDTH - 50); // keep the relais engaged for the THREASHOLD time, minus the time that we've spent on flashing thr coin led
        digitalWrite(RELAIS, LOW);
        digitalWrite(RELAIS_STATUS_LED, LOW);
      }
    
    }
    
    
    
    
    /* 
      return TRUE when we detect that the IR channel in disturbed (i.e.: a coin is passing through it)
      That is the case when the voltage presented on analog pin IR drops below THREASHOLD.
    */  
      
    bool detectCoin() {
      // measure the voltage of the IR circuit
      int iSensorValue = analogRead(IR);
      
      // debug info
      char output[80];
      sprintf(output, "Sensor: %d\n", iSensorValue);  
      Serial.print(output); 
    
      // if the detected voltage is below THREASHOLD, a coin is passing through the channel  
      return (iSensorValue < THREASHOLD); // there is something in the IR path
    }

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • doctorcdf
    doctorcdf over 11 years ago in reply to Jan Cumps

    Jan -

     

    If you're willing to blog about the project, we'll be happy to look at supplying you the parts.  The "Internet of Cola" isn't a bad title (thanks Peter!)

     

    Best Regards, Christian

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • doctorcdf
    doctorcdf over 11 years ago in reply to Jan Cumps

    Jan -

     

    If you're willing to blog about the project, we'll be happy to look at supplying you the parts.  The "Internet of Cola" isn't a bad title (thanks Peter!)

     

    Best Regards, Christian