Robotics
  • Technologies
  • More
Robotics
Blog Robot uses small explosions to leap vertically into the air
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Robotics to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 15 Feb 2013 9:37 PM Date Created
  • Views 742 views
  • Likes 0 likes
  • Comments 1 comment
  • research
  • industrial
  • hmi
  • robotics
  • robots
  • control
  • motion_control
  • robot
  • on_campus
  • motion
  • cabeatwell
  • soft_robot
  • university
  • alternative_motion
  • innovation
  • navigation
Related
Recommended

Robot uses small explosions to leap vertically into the air

Catwell
Catwell
15 Feb 2013

image

Height comparison (via Harvard)

 

Soft robots (flexible) have several methods of locomotion that includes walking, crawling and rolling but now researchers from Harvard and Cornell University have added another method that involves small explosions. The researchers, led by assistant professor (from Cornell University) Robert Shepherd, designed a 3-legged soft robot that’s capable of leaping a foot into the air by capitalizing on a small-scale internal explosion. To design the robot the team used a 3D printer to fabricate the robot’s body, which is made from soft pliable silicon. This allows the form to contort in a variety of positions with relative ease over rigid plastics, which allows the robot to move in limited spaces at a quick pace. To get the robot to jump the team installed a series of tubes that deliver a precise amount of oxygen and hydrogen to hollow channels in each of the robots legs.

 

image

The soft robot igniting the reaction. Flames shoot down channels of the extremities. This enables the bot to just many times its height. (via Harvard demo video)

 

The gas mixture is “lit” using wires that generate an electrical current, which is regulated by a simple valve actuator. Heat generated by the ignited gas forces a flap (on each leg) to close which pressurizes the leg and causes it to actuate. Once the gas cools, the flap opens back up and more gas is piped in to expel the exhaust. While some may think that the explosions and heat would inherently damage the soft robot, the detonation is actually so short that the soft silicon is able to absorb the energy with relative ease. It can even handle the heat as the research team found that, over time, the resulting build-up of heat was less than 1 Kelvin after prolonged detonations. While the robot is limited in range due in part by being tethered by gas tubing and electrical wiring, they hope to develop their robot with a fully contained energy system, which would be a prerequisite for applications such as search and rescue operations sometime in the future. They would also have to figure out a way for the robot to travel in different directions either autonomously or by RC, otherwise it will be limited in most applications. First step’s first.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Cabe

http://twitter.com/Cabe_e14

  • Sign in to reply
Parents
  • DAB
    DAB over 13 years ago

    I am having a lot of trouble trying to visualize where this type of robot would have any place in a real world environment.

     

    I guess if you can have bacteria generate the oxygen and hydrogen from water, then I could see it working in a water environment, but if it needs to consume energy to move, then I cannot see an application where it would be better than a conventional robot.

     

    Anybody have any ideas?  What am I missing?

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 13 years ago

    I am having a lot of trouble trying to visualize where this type of robot would have any place in a real world environment.

     

    I guess if you can have bacteria generate the oxygen and hydrogen from water, then I could see it working in a water environment, but if it needs to consume energy to move, then I cannot see an application where it would be better than a conventional robot.

     

    Anybody have any ideas?  What am I missing?

     

    DAB