Robotics
  • Technologies
  • More
Robotics
Blog ROS2 Learning Series - Blog 5 - Basic Programming - Part 2
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Robotics to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: crisdeodates
  • Date Created: 9 Apr 2024 1:41 PM Date Created
  • Views 1008 views
  • Likes 4 likes
  • Comments 4 comments
  • Robot operating System
  • robotics
  • ROS2
  • ROS
Related
Recommended

ROS2 Learning Series - Blog 5 - Basic Programming - Part 2

crisdeodates
crisdeodates
9 Apr 2024
ROS2 Learning Series - Blog 5 - Basic Programming - Part 2

ROS2 Service - Client Server Project

In the previous blog, we saw how to create a publisher subscriber project.

This project makes remakes it into a service based client server project.

For developing a service, a service package needs to be created using ament_cmake build tool. 

Go to the src folder in the root of the workspace and create a package called ‘sum_nums_srv’ using ament_cmake. 

$ cd ~/ros2_ws/src 
$ ros2 pkg create --build-type ament_cmake sum_nums_srv 

 

If we look at the directory structure of the new package ‘sum_nums_srv’, we can see that there is an include and src folder which we don't need. We will add a srv folder to place our service structure file called ‘SumNumsSrv.srv’. 

$ cd sum_nums_srv 
$ rm -rf include src 
$ mkdir srv 
$ cd srv 
$ touch SumNumsSrv.srv 

 

NOTE: A service structure file is treated as an interface file in ROS2 and hence needs to start with a Capital letter. 

 

Now our package ‘sum_nums_srv’ folder should look like the following structure: 

sum_nums_srv/ 
├── CMakeLists.txt 
├── package.xml 
└── srv 
    └── SumNumsSrv.srv 

 

Populate the srv file with the following service request and response structure and save it: 

int8 n 
--- 
int64 sum 

This srv file informs ROS2 that this service will request an integer n, and responds with an integer called sum. 

 

To convert the service interfaces into language-specific code (like C++ and Python) we should add the following lines to CMakeLists.txt, including any dependencies if any: 

find_package(rosidl_default_generators REQUIRED) 
 
rosidl_generate_interfaces(${PROJECT_NAME} 
  "srv/SumNumsSrv.srv" 
) 

 

Add the following lines within the <package> element of package.xml: 

<buildtool_depend>rosidl_default_generators</buildtool_depend> 
<exec_depend>rosidl_default_runtime</exec_depend> 
<member_of_group>rosidl_interface_packages</member_of_group> 

Since the interfaces rely on rosidl_default_generators for generating language-specific code, we need to declare a build tool dependency on it. rosidl_default_runtime is a runtime or execution-stage dependency, needed for using the interfaces later. The rosidl_interface_packages is the name of the dependency group that our package, ‘sum_nums_srv’, should be associated with, declared using the <member_of_group> tag. 

 

Build the ‘sum_nums_srv’ package (selecting only the new package). 

$ source install/setup.bash 
$ ros2 interface show sum_nums_srv/srv/SumNumsSrv 

Test the new service. 

$ source install/setup.bash 
$ ros2 interface show sum_nums_srv/srv/SumNumsSrv 

This will display the service structure. 

 

Now go back to our ‘sum_nums’ package and use this newly created service package. 

Create two files called ‘sum_nums_service_server.py’ and ‘sum_nums_service_client.py’ in the same folder as our publisher subscriber files are. 

$ cd src/sum_nums/sum_nums 
$ touch sum_nums_service_server.py sum_nums_service_client.py 

 

Populate the sum_nums_service_server.py file with the service server code: 

from sum_nums_srv.srv import SumNumsSrv 
import rclpy 
from rclpy.node import Node 
 
class SumNumsClient(Node): 
    """ 
    Node to send requests to compute the sum of first n integer numbers. 
    """ 
    def __init__(self): 
        """ 
        Initializes the SumNumsClient class. 
        """ 
        super().__init__('sum_nums_client_node') 
        self.cli = self.create_client(SumNumsSrv, 'sum_n_nums') 
        while not self.cli.wait_for_service(timeout_sec=1.0): 
            self.get_logger().info(' SumNumsSrv service not available, waiting...') 
        self.req = SumNumsSrv.Request() 
 
    def send_request(self, n): 
        """ 
        Sends a request to compute the sum of first n integer numbers. 
 
        Parameters: 
            n: The number of integer numbers to sum. 
 
        Returns: 
            The response containing the computed sum. 
        """ 
        self.req.n = n 
        self.future = self.cli.call_async(self.req) 
        rclpy.spin_until_future_complete(self, self.future) 
        return self.future.result() 
 
def main(args=None): 
    """ 
    Main function to initialize the node and send a request to compute the sum of first n integer numbers. 
    """ 
    rclpy.init(args=args) 
 
    sum_nums_client_node = SumNumsClient() 
 
    num_input = int(input("Enter a positive integer number: ")) 
    if num_input < 0: 
        print("Input number is not positive") 
    else: 
        print('Entered:', num_input) 
        response = sum_nums_client_node.send_request(num_input)     
        print("Sum of first", num_input, "integer numbers is:", response.sum) 
 
    # Destroy the node explicitly 
    sum_nums_client_node.destroy_node() 
    rclpy.shutdown() 
 
if __name__ == '__main__': 
    main() 

 

Populate the sum_nums_service_client.py file with the service client code: 

from sum_nums_srv.srv import SumNumsSrv 
import rclpy 
from rclpy.node import Node 
 
class SumNumsClient(Node): 
    """ 
    Node to send requests to compute the sum of first n integer numbers. 
    """ 
    def __init__(self): 
        """ 
        Initializes the SumNumsClient class. 
        """ 
        super().__init__('sum_nums_client_node') 
        self.cli = self.create_client(SumNumsSrv, 'sum_n_nums') 
        while not self.cli.wait_for_service(timeout_sec=1.0): 
            self.get_logger().info(' SumNumsSrv service not available, waiting...') 
        self.req = SumNumsSrv.Request() 
 
    def send_request(self, n): 
        """ 
        Sends a request to compute the sum of first n integer numbers. 
 
        Parameters: 
            n: The number of integer numbers to sum. 
 
        Returns: 
            The response containing the computed sum. 
        """ 
        self.req.n = n 
        self.future = self.cli.call_async(self.req) 
        rclpy.spin_until_future_complete(self, self.future) 
        return self.future.result() 
 
def main(args=None): 
    """ 
    Main function to initialize the node and send a request to compute the sum of first n integer numbers. 
    """ 
    rclpy.init(args=args) 
 
    sum_nums_client_node = SumNumsClient() 
 
    num_input = int(input("Enter a positive integer number: ")) 
    if num_input < 0: 
        print("Input number is not positive") 
    else: 
        print('Entered:', num_input) 
        response = sum_nums_client_node.send_request(num_input)     
        print("Sum of first", num_input, "integer numbers is:", response.sum) 
 
    # Destroy the node explicitly 
    sum_nums_client_node.destroy_node() 
    rclpy.shutdown() 
 
if __name__ == '__main__': 
    main() 

 

Add the entry points to setup.py inside console_scripts section: 

'sum_nums_server = sum_nums.sum_nums_service_server:main', 
'sum_nums_client = sum_nums.sum_nums_service_client:main', 

 

Since our ‘sum_nums’ package depends on ‘sum_nums_srv’ package for the service structure, add it as a dependency inside the package.xml file: 

<exec_depend>sum_nums_srv</exec_depend> 

 

Build the ‘sum_nums’ package again. 

$ cd ~/ros2_ws/ 
$ colcon build --packages-select sum_nums 
$ source install/setup.bash 

Execute the service node in the same terminal window. 

$ ros2 run sum_nums sum_nums_server 

 

Execute the client node in a new terminal window. 

$ source install/setup.bash 
$ ros2 run sum_nums sum_nums_client 

Enter a positive integer number and press Enter. 

The sum will be displayed by the sum_nums_client node. 

image

  • Sign in to reply
  • crisdeodates
    crisdeodates over 2 years ago in reply to DAB

    Usually we wrap these complex data types as custom messages in ROS which are used in those particular cases.
    I will definitely cover them in the future blogs. Thanks for the suggestion DAB  Slight smile

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 2 years ago in reply to crisdeodates

    Most projects use complex data structures mixing integer, floating point, boolean and character data.

    When you are running distributed and parallel computing applications, you need to send multiple data and types between computers for information and status transfers.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • crisdeodates
    crisdeodates over 2 years ago in reply to DAB

    Yes DAB Could you give some examples?
    I am also working on publishing some advanced projects as part of this series.
    May be I can try to include your recommendations as well Slight smile

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 2 years ago

    I assume you can use more complex data structures?