Robotics
  • Technologies
  • More
Robotics
Blog Scientists win Nobel Prize in physics with their creation of blue LEDs
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Robotics to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 9 Oct 2014 2:48 AM Date Created
  • Views 1201 views
  • Likes 0 likes
  • Comments 2 comments
  • nobel
  • nobel_prize
  • lighting
  • on_campus
  • blue_led
  • led
  • cabeatwell
  • akasaki
  • university
  • isamu
  • innovation
Related
Recommended

Scientists win Nobel Prize in physics with their creation of blue LEDs

Catwell
Catwell
9 Oct 2014

image

Sure, they’re blue but we can’t have white light without them (via wiki)

 

Eons ago (roughly 1907), scientists began messing with the idea of LEDs in the form of electroluminescence using a crystal of silicon carbide and a cat’s-whisker detector. Apparently, Edison’s light bulb was no longer cutting the mustard and people wanted tiny little lights in their radios, which is probably why RCA was playing around with gallium arsenide-based semiconductors back in 1955.


Regardless, LEDs have come a long way in the last hundred years and has become the dominant light source on the planet overtaking incandescent and fluorescent lighting. While the LEDs manufactured today are highly efficient, energy saving and environmentally friendly, they do have their drawbacks, in this case the ability to generate a broad spectrum of colors. More specifically, white light due to the fact scientists couldn’t produce blue light in LED form.



image


It’s all in the GaN- gallium nitride revolutionized blue LED lighting paving the way for white (via wiki)


Confused yet? Ok, let’s break it down in simple terms- in order to create bright, efficient white light, green or red LEDs need to be combined with a blue LED. They could also be shown through a phosphor that emits red and green light. Sure there have been blue LEDs in existence since the 70’s but the material they are made from made them pretty much useless in the broad spectrum (pun intended) of practical applications.


By the late 80’s, the peoples demand for bright, shiny things continued to grow and there still were not any devices (much less radios) with tiny LEDs that glowed bright white or blue. Noticing those demands, three material scientists decided the world could wait no longer for bright, efficient blue LEDs and began developing their own using gallium nitride.

 

image

Meijo University Prof. Isamu Akasaki, second right, receives flower bouquet at a news conference after winning the Nobel prize in physics at the university in Nagoya, central Japan. Picture: AP Photo/Kyodo News. Source: AP

 

In the early 90’s, Professors Isamu Akasaki (Nagoya University), Hiroshi Amano (Nagoya University) and Shuji Nakamura (University of California) began working on a way to grow gallium crystals big enough to be used to emit blue light. They found that they could do so using a specially designed scaffold made in part with sapphire. That’s the key, different materials emit a different colored light when applied to LEDs and gallium was the ticket in emitting blue.


Gallium isn’t without its troubles as it tends to become poisoned when exposed to hydrogen. The people would have to wait a few years more before they would get bright, shiny blue or white lights. To get around that issue, the scientists ‘doped’ up the gallium using aluminum or zinc but ultimately went with indium, which protects the gallium from the hydrogen used in manufacturing the semiconductor the LED resides on.


The hard work that all three endeavored over the years to get an efficient blue LED earned the trio a Nobel Prize this year in physics. Not only does their work provide bright and shiny LEDs in our mobile devices but also reduces the power draw on the grid when used for lighting our homes. Not only that, they are also better for the environment over compact florescent lighting (CFLs) due to the fact that the latter is filled with mercury. The trio will receive their prizes in Stockholm in December, where their breakthroughs will be seen lighting up the homes all over the city.


C

See more news at:

http://twitter.com/Cabe_Atwell

  • Sign in to reply
Parents
  • DAB
    DAB over 11 years ago

    Hi Cabe,

     

    You might add that the interest in Blue light at the time was to reduce the optical digits for CDROMs.  Blue light is half the wavelength of red light, so just by changing the LED, you could double the data density.

    The push now is to go into the UV wavelengths.

    We will see who makes the first breakthrough.

     

    DAB

     

    PS did you ever write you review of my book?

    Just curious.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 11 years ago

    Hi Cabe,

     

    You might add that the interest in Blue light at the time was to reduce the optical digits for CDROMs.  Blue light is half the wavelength of red light, so just by changing the LED, you could double the data density.

    The push now is to go into the UV wavelengths.

    We will see who makes the first breakthrough.

     

    DAB

     

    PS did you ever write you review of my book?

    Just curious.