Robotics
  • Technologies
  • More
Robotics
Blog Spider bots in the blood stream
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Robotics to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Eavesdropper
  • Date Created: 12 Sep 2011 9:19 PM Date Created
  • Views 785 views
  • Likes 1 like
  • Comments 1 comment
  • research
  • robotics
  • robots
  • control
  • robot
  • on_campus
  • behavior
  • eavesdropper
  • school
  • Health
  • university
  • medical
  • automation
  • innovation
Related
Recommended

Spider bots in the blood stream

Eavesdropper
Eavesdropper
12 Sep 2011
Dr. Octopus to the rescue! Coming soon from Penn State University science department....The amazing Micro-Spider Bots: Why are they amazing you might ask? Inventor Ayusman Sen hopes to attach the spider bots to other nanobots to perform tasks within the human body. Which could be used to detect tumors, bolster the immune system and clear vessels clean of plaque.
The Micro-Spider bots  are made of two spheres, one gold, the other silica, and measure less than a micrometer wide. For comparison, the average blood cell is 6 to 10 micrometers wide.
 
The spider bots are self-propelled by a molecule called the Grubbs catalyst, a molecule that makes chains of smaller molecules, like a spider spinning its web. When placed in a container of the chemical norborene, the catalyst "spins a polymer" of molecules from the chemical. With more unpolymerised molecules on the gold side, the solvent moves into that region creating a flow. This, in turn, creates movement of the spider itself. Movement is controllable.
 
The team  put down a trail norborene in a solvent, and the spider bots followed the path. This could lead to guiding the bots to a site of infection. This concept is nothing  really new; however, it is the advancement in the field of nano-medical robotics. I hope they come up with a better name the spider bots because people might be a little uncomfortable getting injected with spiders.
 
The next step is to create a series of Spider-bots that can be powered off glucose or other chemical available readily in the body.
 
Eavesdropper
  • Sign in to reply
Parents
  • DAB
    DAB over 15 years ago

    It looks like medical nanobots may soon be a reality.  I can see this level of technology used in veternary procedures and non-medical applications.  They could use these bots to look into sewer system leaks, inspect plumbing, and all kinds of small detail required functions.

     

    I could also see these bots used in medical emergency treatments, where they could be sprayed on a wound, where they could lock together to form a temporary field dressing and stop blood and fluid loss.  They could save a lot of lives very soon.

     

    Thanks

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 15 years ago

    It looks like medical nanobots may soon be a reality.  I can see this level of technology used in veternary procedures and non-medical applications.  They could use these bots to look into sewer system leaks, inspect plumbing, and all kinds of small detail required functions.

     

    I could also see these bots used in medical emergency treatments, where they could be sprayed on a wound, where they could lock together to form a temporary field dressing and stop blood and fluid loss.  They could save a lot of lives very soon.

     

    Thanks

    DAB