Robotics
  • Technologies
  • More
Robotics
Blog Spot CNC repair robot for hazardous environments, the Mini-RoboMach
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Robotics to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 30 Jan 2013 8:35 PM Date Created
  • Views 733 views
  • Likes 1 like
  • Comments 1 comment
  • research
  • transportation
  • Hexapod
  • industrial
  • industry
  • manufacturing
  • robotics
  • field_engineer
  • robot
  • cnc
  • field_tech
  • cabeatwell
  • prototyping
  • field_technician
  • milling
  • mill
  • tools
  • machine_vision
  • sensor
  • innovation
  • hexapod_machining
Related
Recommended

Spot CNC repair robot for hazardous environments, the Mini-RoboMach

Catwell
Catwell
30 Jan 2013

image

Mini-RoboMach concept in a "hybrid configuratin," with "free-hex" and "snake-arm." (via Mechatronics)

 

The automation of machining tools ranges in application from something as simple as remotely drilling a hole to a more complex task of assembling machinery equipment. With the development of autonomous robots, the unification of these two technologies is a favorable move. People are often put into harm’s way when hazardous environments such as nuclear power plants go under maintenance. Now, a European consortium is working on a project that may revolutionize the way on-site repair is done in these types of environments.

 

 

The MiRoR project aims to develop a Miniaturized Robotic Machine (Mini-RoboMach) that will perform “holistic in-situ” repair to various installations and industrial complexes in otherwise hard to reach areas. Industries such as energy plants and oil drilling stations will benefit from such a system by keeping their valiant workers out of danger. The consortium is already backed by the support of the University of Nottingham, Rolls Royce, The Swiss Federal Institute of Technology, AREVA, Acciona Infrastructure, and Petrom - giving the project access to patented technology and a head start on industrial application partners.

 

image

Prototype Mini-RoboMach (via Mechatronics)

 

 

The CNC robot makes use of the novel “free-leg hexapod” system, arming it with a six-legged base for performing precision machining processes while on the move. A stiffness-controlled flexible robot arm also gives the system the ability to “snake” and work on a variety of maintenance tasks. Additionally, the Mini-RoboMach integrates a three-level system hierarchy to control its functions. The low-level directs the machining processes, while the intermediate-level governs the system’s movements. The high-level functions are related to the intelligent controls, which give the robot navigation guidelines in addition to inspecting and analyzing its surrounding environment for optimal leg positioning and machine calibration prior to performing the required task.

 

 

Once the autonomous CNC machine is developed, further work will be done to evaluate its performance. A virtual workbench will be created to pre-assess the robot’s hardware and software prior to demonstrating its usefulness on large, intricate industrial environments.

 

 

Cabe

http://twitter.com/Cabe_e14

  • Sign in to reply
  • DAB
    DAB over 13 years ago

    People have been speculating about nanites repairing humans from within for a couple of decades.  I see the development of the CNC type robot as a step towards further miniturization.

    It makes a lot of sense to start looking at the utility of these types of robots and get the prototypes into the field so we can begin to learn all of the little details that need to be cleaned up before we can begin to see minibots supporting everyday tasks.

     

    In many ways, this is an exciting time for robot builders.  You now have a much broader acceptance of robots working in society and communities.  You also have the fear of losing your job to a robot greatly deminished given the actual requirements for emplying these types of robots.

     

    The coming years will yield an interesting evolution of how robots leave the factory floor and begin to enter everyday communities.

     

    Neat.

    DAB