Robotics
  • Technologies
  • More
Robotics
Blog Swann’s RC Choppers, iDevice control on the cheap
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Robotics to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 2 Feb 2012 8:27 PM Date Created
  • Views 770 views
  • Likes 1 like
  • Comments 4 comments
  • hmi
  • robotics
  • robots
  • control
  • telepresence
  • cell_phone
  • robot
  • cabeatwell
  • ios
  • idevice
  • innovation
  • navigation
  • iphone
Related
Recommended

Swann’s RC Choppers, iDevice control on the cheap

Catwell
Catwell
2 Feb 2012
image
 
The days of the old RC car are certainly fading, especially when you see the RC helicopters and quad-copters showing no constraint to the ground. Like many other RC toys, three new controllable vehicles from Swann allow control via iDevices (iPad, iPod and iPhone). Swann has three new helicopters, the iFly Micro Lightning, the SkyEye and the Black Swann that will grant you this level of fun and more for less than $100.
 
All three helicopters include dual joystick IR remotes that require 6 AA batteries but can also be controlled using and iDevice with the included attachment and Swann application. They come with lithium batteries that can be recharged from the remotes or with an included USB cable from a PC. They all have Swann’s Easy-fly Gyro Technology, trim adjustment for stabilization to maximize performance during the 8-minute flight allowed by a charge.
 
For those of you with an agenda, two of the helicopters have onboard wireless cameras that take pictures and video on remote command. The SkyEye includes 512 MB of memory while the Black Swann has space for a 32 GB micro SD card. These two helicopters have 27 MHz frequency controllers that range for 110 ft.
 
The iFly Micro Lightning goes for $69.99 and the SkyEye and Black Swann sell for $99.99. Added rotors and a helipad game are included for inevitable accidents and to practice before you embark on your first adventure.
 
Below is an example of the video output of these helicopters. Seems usable.
This video is unavailable.
You don't have permission to edit metadata of this video.


Cabe
http://twitter.com/Cabe_e14
  • Sign in to reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to DAB

    Actually 8 min for that size of chopper is pretty good. Most that size only run for 6 min on average. The little choppers use a 3.7V Lipo battery. Most are only rated at 150mAh to 180mAh. You could add a second battery in parallel for longer battery life. But the main problem with this size of chopper is you can't effectively use them outside. Any amount of wind throws them around like paper airplanes. Sure teh video shows it flying outside but i doubt there was any wind the day they made that video. If you want more fly time then get a bigger chopper.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to DAB

    The battery size and capacity are limited to size of that, bigger battery can't be lifted. It's almost the maximum size.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Eavesdropper
    Eavesdropper over 14 years ago in reply to DAB

    As the super capacitor charge density increases, so will the flight time for these RC vehicles.

     

    Just a matter of time.

     

    E

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 14 years ago

    Hi Cabe,

     

    They look interesting but why are they limited to 8 minutes of flighy?  I would be looking for something at least 30 minutes to an hour for a reasonable mapping requirement.

     

    Thanks for the info, I might give them a call and see where they are going in the future.  Hang time is definately a need.

     

    DAB