Robotics
  • Technologies
  • More
Robotics
Blog The First Hoverboard wins Kickstarter - could mark the end of the wheel
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Robotics to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 25 Nov 2014 6:26 PM Date Created
  • Views 571 views
  • Likes 0 likes
  • Comments 1 comment
  • magnetic
  • hendo_hover
  • tony_hawk
  • skateboard
  • cabeatwell
  • hoverboard
  • magnets
  • mag_lev
  • lev
Related
Recommended

The First Hoverboard wins Kickstarter - could mark the end of the wheel

Catwell
Catwell
25 Nov 2014

image

The first hoverboard created by Hendo and up on Kickstarter (via Hendo Hover)


Hold the phone and take me Back to the Future! Someone has created a real hoverboard! Recently, there was a big hub bub about a Back to the Future electric skateboard commemorating the awesomeness of Marty McFly. That is no comparison to an actual hoverboard!

 

Actually, I should preface this with the fact that you won’t be riding a hoverboard to work in the near future, but we could be driving hover-cars in 5 years, maybe. I can dream, at least.

 

Hendo is a start-up that was inspired to make a long-time dream a reality. The Kickstarter campaign is still up and running with 31 days to go and they have already received almost double their pledged goal. This hoverboard project currently has over $440,000 in funding! It's safe to say, people are going bananas for hoverboards.

 

So, how does this baby work? Well, it only hovers one inch off the ground, but that's a lot more than any other piece of furniture I own. The board floats using four, disk-shaped, hover engines which are located underneath the board. These 'engines' create a magnetic field that allows the board to hover and move above a surface with no friction. It is a technology similar to electromagnetic trains that hover above their tracks. However, this technology is scalable and doesn't need tracks, per say.

 

The setback is that the hoverboard needs to use a non-ferromagnetic conductor as a surface substrate. Hence, this board isn't going to be hovering over city sidewalks anytime soon, but Hendo has built their own skate park for their hoverboard. They plan to build parks like that around different cities to allow hoverboard owners to play to their hearts content. If you want a fully functioning hoverboard, I'm afraid you're out of luck for now. The boards are already sold to 11 lucky backers for $10,000 a pop.

 

But for you makers and tinkers out there, Hendo is offering really affordable tinker kits with the hover technology on Kickstarter which allows you to hover just about anything and make it fit your needs. Personally, I'm thinking of hovering my morning coffee to myself. While the basic kit allows you to take the technology apart and play with it, their Whitebox+ is a fully functional hovering box that you can remote control with your smartphone. While this isn't meant to be tinkered with, it could become a robot waiter of sorts. At the very least, it will resemble the footrest from Beauty and the Beast.

 

While Hendo isn't exactly offering ready-made hoverboards yet, their main reason for needing funding is to develop what they are calling Magnetic Field Architecture (MFA). This technology is what allows the hoverboard to work, and is less expensive and more sustainable than current magnetic propulsion technology. Hendo is hoping to develop this technology to the point that you could virtually make any and everything hover anywhere. I'm really hoping that they succeed in developing this technology way beyond a simple hoverboard so that I can hover above the giant Chicago pot holes that attempt to eat my car every winter.


You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image


C

See more news at:

http://twitter.com/Cabe_Atwell

  • Sign in to reply
  • michaelkellett
    michaelkellett over 11 years ago

    OK - it's all whizzo and fun but now it's time to engage brain.

     

    Why don't we all use magnetic levitation for everything - because it uses power just to keep still. And these people are not saying how much power - but that's the ONLY parameter that matters. They might be able to make some skate parks but don't expect trains, or anything much other than toys, any time soon.

     

    MK